<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using usbdm library in custom projects in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461358#M21693</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Edward.&lt;/P&gt;&lt;P&gt;Yes, now I can read device (I'm working with GB60 MCU), using C# wrapper for usbdm library from the usbdm project of pgo. But example (here the link: &lt;A href="http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_CF_JMxx/html/usbdm_programming.html#USBDM"&gt;http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_CF_JMxx/html/usbdm_programming.html#USBDM&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;is very simple and there is not example of using that library for erase and write MCU. I try to read datasheet, but can not understand how to use that library... If I can see any simple example for using that library, it can be easy for me in my project.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jan 2016 21:32:05 GMT</pubDate>
    <dc:creator>yarik111475</dc:creator>
    <dc:date>2016-01-29T21:32:05Z</dc:date>
    <item>
      <title>Using usbdm library in custom projects</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461356#M21691</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyine.&lt;/P&gt;&lt;P&gt;English is not my native lang., so I excuse for any mistakes.&lt;/P&gt;&lt;P&gt;The problem is that. I try to use the usbdm.4.dll library in custom programming project for read/write mcu HCS08 series (I programming in C#).&lt;/P&gt;&lt;P&gt;Now I can read device, but just have not idea how to write device's memory to using this library.&lt;/P&gt;&lt;P&gt;Maybe someone has some custom working project using that .dll (they may be on C or C++, I can understand them).&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 13:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461356#M21691</guid>
      <dc:creator>yarik111475</dc:creator>
      <dc:date>2016-01-25T13:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: Using usbdm library in custom projects</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461357#M21692</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not familiar with usbdm and your USB&amp;lt;-&amp;gt;BDM adapter, but since you can read S08, you also should be able to read write to RAM of your S08 device. Writing to flash memory should be done according to your S08 device flash memory programming algorithm. You can directly manipulate flash module register from BDM, so next step would be to read your S08 datasheet and read about flash module clock initialization and flash erase and program algorithm, which is not the same for all S08 devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jan 2016 08:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461357#M21692</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2016-01-29T08:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: Using usbdm library in custom projects</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461358#M21693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Edward.&lt;/P&gt;&lt;P&gt;Yes, now I can read device (I'm working with GB60 MCU), using C# wrapper for usbdm library from the usbdm project of pgo. But example (here the link: &lt;A href="http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_CF_JMxx/html/usbdm_programming.html#USBDM"&gt;http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_CF_JMxx/html/usbdm_programming.html#USBDM&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;is very simple and there is not example of using that library for erase and write MCU. I try to read datasheet, but can not understand how to use that library... If I can see any simple example for using that library, it can be easy for me in my project.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jan 2016 21:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461358#M21693</guid>
      <dc:creator>yarik111475</dc:creator>
      <dc:date>2016-01-29T21:32:05Z</dc:date>
    </item>
    <item>
      <title>Re: Using usbdm library in custom projects</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461359#M21694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looks like there's more suitable place for questions regarding USBDM API&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/space/2024"&gt;OSBDM and TBDML&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/107724"&gt;Programming with the USBDM API&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that looking there you should find some examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Jan 2016 06:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461359#M21694</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2016-01-30T06:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: Using usbdm library in custom projects</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461360#M21695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Edward, I'll try to ask developer of that library (pgo) over there. May be he will help me with some source code files...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Jan 2016 11:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-usbdm-library-in-custom-projects/m-p/461360#M21695</guid>
      <dc:creator>yarik111475</dc:creator>
      <dc:date>2016-01-30T11:49:11Z</dc:date>
    </item>
  </channel>
</rss>