<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMC9RS08KA2</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460759#M21683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can´t download a empty program to my uC. The hardwire is well done, but Codewarrior cannot be communicate with the uC. What is it happening? The uC it is MC9RS08KA2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Dec 2015 20:00:58 GMT</pubDate>
    <dc:creator>jorgehoraciogon</dc:creator>
    <dc:date>2015-12-31T20:00:58Z</dc:date>
    <item>
      <title>MC9RS08KA2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460759#M21683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can´t download a empty program to my uC. The hardwire is well done, but Codewarrior cannot be communicate with the uC. What is it happening? The uC it is MC9RS08KA2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Dec 2015 20:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460759#M21683</guid>
      <dc:creator>jorgehoraciogon</dc:creator>
      <dc:date>2015-12-31T20:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: MC9RS08KA2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460760#M21684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the configuration used on my side:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CW for MCU v10.6.4 + patches&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; TWR-ELEV + TWR-S08UNIV + TWR-RS08DC-KA8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under CW for MCU v10.6.4 I've created an example for KA8 for OSBDM and P&amp;amp;E connection.&lt;/P&gt;&lt;P&gt;I can connect the TWR-S08UNIV using P&amp;amp;E Multilink Universal Rev B&amp;nbsp; and the example can be downloaded without problem.&lt;/P&gt;&lt;P&gt;Now for the OSBDM, it's another story ... I get some problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However on your side it seems you're using P&amp;amp;E interface and not OSBDM.&lt;/P&gt;&lt;P&gt;Using P&amp;amp;E Multilink Universal Interface I can download the application without problem&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 14:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460760#M21684</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-01-04T14:31:18Z</dc:date>
    </item>
    <item>
      <title>Re: MC9RS08KA2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460761#M21685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33739iEBD15759CC2926B4/image-size/large?v=v2&amp;amp;px=999" title="IMG_20160105_090524.jpg" alt="IMG_20160105_090524.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33812i6C9DD6632B2D6C8A/image-size/large?v=v2&amp;amp;px=999" title="Sin título.jpg" alt="Sin título.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33852iFD8351876087A7F4/image-size/large?v=v2&amp;amp;px=999" title="Sin título1.jpg" alt="Sin título1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hello Pascal!&lt;/P&gt;&lt;P&gt;But I still can´t solve the problem. I´m adding a pic of the hardwire.&lt;/P&gt;&lt;P&gt;The uC is it new, but I think it could be a problem with the Multilink.&lt;/P&gt;&lt;P&gt;Also, I can see the driver in the Device Manager of Windows and appears is it working well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why CW can detect the Multilink and can´t be communicate with the uC if this is new?, do I need to change the Debug Configuration in the CW?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I remark, when I created the Boreboard Project, I selected the right options.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jan 2016 18:30:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460761#M21685</guid>
      <dc:creator>jorgehoraciogon</dc:creator>
      <dc:date>2016-01-05T18:30:08Z</dc:date>
    </item>
    <item>
      <title>Re: MC9RS08KA2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460762#M21686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have an eval board to test the configuration ?&lt;/P&gt;&lt;P&gt;It could be fine to test the configuration (codeWarrior + Multilink).&lt;/P&gt;&lt;P&gt;On my my side it's working fine using Tower kit.&lt;/P&gt;&lt;P&gt;I don't think there is a problem with the Multilink as the 2 leds are switched-on.&lt;/P&gt;&lt;P&gt;The Multulink is detected by CodeWarrior following the Error.png file.&lt;/P&gt;&lt;P&gt;I think there is a problem between the Multilink and the device and this explain the error2.png file.&lt;/P&gt;&lt;P&gt;Most of the time, the message "error2.png" occurs when a wrong power supply is provided on-board or when the Multilink is not correctly connected to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This question is may be more for hardware colleague.&lt;/P&gt;&lt;P&gt;I will move the question to them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pascal&lt;BR /&gt;NXP Technical Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 08:12:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460762#M21686</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2016-01-06T08:12:36Z</dc:date>
    </item>
    <item>
      <title>Re: MC9RS08KA2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460763#M21687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Pascal!&lt;/P&gt;&lt;P&gt;I solved the problem. I downloaded the firmware again and I could burn the uC.&lt;/P&gt;&lt;P&gt;Multilink can't program different families of uC before download the correct firmware.&lt;/P&gt;&lt;P&gt;Thank you and I expect this can help someone else in the future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day too!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 14:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9RS08KA2/m-p/460763#M21687</guid>
      <dc:creator>jorgehoraciogon</dc:creator>
      <dc:date>2016-01-06T14:33:00Z</dc:date>
    </item>
  </channel>
</rss>