<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TWR-MCF51CN Bootloader Mode problem in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/459988#M21672</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I have TWR-MCF51CN board and I have problem with bootloader mode in it. When I want to update my firmware by P&amp;amp;E firmware updater I have to use jumper on J16. When I've done it my device become undetected. When I use CodeWarrior v10.6.4 it also makes update of my firmware and it's the same problem. It happens when I reconnect my board with jumper on. Without jumper on J16 my device is detected. I'm using Mini USB cable as debugger.&lt;BR /&gt;Thanks for all responses.&lt;BR /&gt;Greetings,&lt;BR /&gt;Pawel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Dec 2015 16:21:18 GMT</pubDate>
    <dc:creator>pawelniewiadoms</dc:creator>
    <dc:date>2015-12-03T16:21:18Z</dc:date>
    <item>
      <title>TWR-MCF51CN Bootloader Mode problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/459988#M21672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I have TWR-MCF51CN board and I have problem with bootloader mode in it. When I want to update my firmware by P&amp;amp;E firmware updater I have to use jumper on J16. When I've done it my device become undetected. When I use CodeWarrior v10.6.4 it also makes update of my firmware and it's the same problem. It happens when I reconnect my board with jumper on. Without jumper on J16 my device is detected. I'm using Mini USB cable as debugger.&lt;BR /&gt;Thanks for all responses.&lt;BR /&gt;Greetings,&lt;BR /&gt;Pawel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 16:21:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/459988#M21672</guid>
      <dc:creator>pawelniewiadoms</dc:creator>
      <dc:date>2015-12-03T16:21:18Z</dc:date>
    </item>
  </channel>
</rss>