<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックHow to set the Bus Clock with 4Mhz</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459795#M21656</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a S08AW16A controller with a external source clock of 4Mhz. I need to set the BUS Clock with 4Mhz. Any suggestions guys.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Dec 2015 13:23:42 GMT</pubDate>
    <dc:creator>gopinatharaveti</dc:creator>
    <dc:date>2015-12-30T13:23:42Z</dc:date>
    <item>
      <title>How to set the Bus Clock with 4Mhz</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459795#M21656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a S08AW16A controller with a external source clock of 4Mhz. I need to set the BUS Clock with 4Mhz. Any suggestions guys.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Dec 2015 13:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459795#M21656</guid>
      <dc:creator>gopinatharaveti</dc:creator>
      <dc:date>2015-12-30T13:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to set the Bus Clock with 4Mhz</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459796#M21657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What programming language do you use? You should read:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/data_sheet/MC9S08AC16.pdf?fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.nxp.com/files/microcontrollers/doc/data_sheet/MC9S08AC16.pdf?fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.nxp.com/files/microcontrollers/doc/data_sheet/MC9S08AC16.pdf?fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCA…&lt;/A&gt; &lt;/P&gt;&lt;P&gt;from page 127&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I give a little help ...&lt;/P&gt;&lt;P&gt;ICGC1 = 0xA0&lt;/P&gt;&lt;P&gt;ICGC2 = 0x00&lt;/P&gt;&lt;P&gt;Check ICGS1 register. You should wait for CLKST0:1 = 1: 0, and the bit REFST = 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have not programmed on the chip but I think you go out there on track.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Saludos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Dec 2015 03:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459796#M21657</guid>
      <dc:creator>Leojunin</dc:creator>
      <dc:date>2015-12-31T03:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: How to set the Bus Clock with 4Mhz</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459797#M21658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using assembly language. I have already been through the data sheet. Below are my configurations to set a 4MHz Bus clock from a 4MHz Ext Source Clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ICGC1_INIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; equ %01011010&amp;nbsp;&amp;nbsp; ; Select FBE (FLL bypassed external i.e., Ext. XTAL/R) and disable loss of clock&lt;/P&gt;&lt;P&gt;ICGC2_INIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; equ %00000001&amp;nbsp;&amp;nbsp; ; Thus ICGOUT = (4MHz * 4)/2 = 8MHz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Dec 2015 08:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459797#M21658</guid>
      <dc:creator>gopinatharaveti</dc:creator>
      <dc:date>2015-12-31T08:28:27Z</dc:date>
    </item>
    <item>
      <title>Re: How to set the Bus Clock with 4Mhz</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459798#M21659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ICGC1 = %10110000 or $B0&lt;/P&gt;&lt;P&gt;HGO should be 1 because it is a higher frequency to 1MHz&lt;/P&gt;&lt;P&gt;RANGE is indistinct because not use the FLL&lt;/P&gt;&lt;P&gt;REFS = 0 is external clock oscilator; REFS = 1 External crystal or resonator&lt;/P&gt;&lt;P&gt;CLKS = 1:0, It is true! I was wrong to read.&lt;/P&gt;&lt;P&gt;The last two to yours taste.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ICGC2 = $00&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Dec 2015 17:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-the-Bus-Clock-with-4Mhz/m-p/459798#M21659</guid>
      <dc:creator>Leojunin</dc:creator>
      <dc:date>2015-12-31T17:02:19Z</dc:date>
    </item>
  </channel>
</rss>