<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic P&amp;E Micro USB Multilink problem with MC908QG8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P-E-Micro-USB-Multilink-problem-with-MC908QG8/m-p/458356#M21636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have a rev. C USB Multilink. P/N is USB-ML-12E. We have been using it several years successfully with a custom designed eval board that has a MC908QG4 part. It has wire wrap headers and a 3 volt regulator on&amp;nbsp; board. Recently I changed the part to a MC908QG8. With the latest version of CodeWarrior open when I connect the 2x3 connector from the Multilink the blue LED is on but the yellow flashes on for a half second and goes out. When I try to flash the part CodeWarrior says there is a connection error. I have changed the QG8 part several several times and the yellow LED never stay on solid. I have verified 3 volts on the BDM connector on the board. We are right in the middle of a project and urgently need help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paul &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Aug 2015 15:40:36 GMT</pubDate>
    <dc:creator>paul_1951</dc:creator>
    <dc:date>2015-08-23T15:40:36Z</dc:date>
    <item>
      <title>P&amp;E Micro USB Multilink problem with MC908QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P-E-Micro-USB-Multilink-problem-with-MC908QG8/m-p/458356#M21636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have a rev. C USB Multilink. P/N is USB-ML-12E. We have been using it several years successfully with a custom designed eval board that has a MC908QG4 part. It has wire wrap headers and a 3 volt regulator on&amp;nbsp; board. Recently I changed the part to a MC908QG8. With the latest version of CodeWarrior open when I connect the 2x3 connector from the Multilink the blue LED is on but the yellow flashes on for a half second and goes out. When I try to flash the part CodeWarrior says there is a connection error. I have changed the QG8 part several several times and the yellow LED never stay on solid. I have verified 3 volts on the BDM connector on the board. We are right in the middle of a project and urgently need help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paul &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Aug 2015 15:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P-E-Micro-USB-Multilink-problem-with-MC908QG8/m-p/458356#M21636</guid>
      <dc:creator>paul_1951</dc:creator>
      <dc:date>2015-08-23T15:40:36Z</dc:date>
    </item>
    <item>
      <title>Re: P&amp;E Micro USB Multilink problem with MC908QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P-E-Micro-USB-Multilink-problem-with-MC908QG8/m-p/458357#M21637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would highly suggest checking the BDM circuit on your target board.&lt;/P&gt;&lt;P&gt;The attached is the schematic of DEMO9S08QG8, to be frank, even only connect pin 1,2,4,6 to the target MCU (MC9S08QG8), both LEDs on USB-Multilink should light and the application can also be programmed!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2015 03:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P-E-Micro-USB-Multilink-problem-with-MC908QG8/m-p/458357#M21637</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2015-08-26T03:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: P&amp;E Micro USB Multilink problem with MC908QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P-E-Micro-USB-Multilink-problem-with-MC908QG8/m-p/458358#M21638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This was a custom demo board I designed. I have come to the conclusion the parts are bad and are getting them replaced.&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 02:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P-E-Micro-USB-Multilink-problem-with-MC908QG8/m-p/458358#M21638</guid>
      <dc:creator>paul_1951</dc:creator>
      <dc:date>2015-08-31T02:04:36Z</dc:date>
    </item>
  </channel>
</rss>