<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic BeeStack: Wakeup other than Keyboard interrupt in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Wakeup-other-than-Keyboard-interrupt/m-p/450114#M21603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using since a long time a system based on MC13213.&lt;/P&gt;&lt;P&gt;It is composed by an "End point" which send periodic data when a BP is pressed (else go to sleep and wakeup with KeyBoard interrupt)&lt;/P&gt;&lt;P&gt;And a coordinator which received data and make action accoding its. (Ack is sent to the end point)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So this system is very simple!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To do this, I started with the exemple MyWirelessAppDemoNonBeaconEndDevice &amp;amp; MyWirelessAppDemoNonBeaconCoordinator&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since last week, I update the system with the last beestack version 3.0.2: BeeKit HCS08 MAC Codebase 2.6.1&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All is ok, but now, the "end point" also Wake up periodically (about 3 or 4 seconds)&lt;/P&gt;&lt;P&gt;It seems to me this is due to a functionnality which I don't remember if exist on my Old stack. This is called "indirect data": Data send by coordinator when end point is in sleeping..&lt;/P&gt;&lt;P&gt;I desactivate all managment of MLME in end point. But may be I forget something?&lt;/P&gt;&lt;P&gt;May be the problem come from other...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then I don't find any way to desactivate a periodic wakeup. (I don't know at this time if it is the Transceiver or the µC timer which Wake up the µC&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;cPWR_DeepSleepMode is set to 1&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 May 2015 18:24:38 GMT</pubDate>
    <dc:creator>arnogir</dc:creator>
    <dc:date>2015-05-20T18:24:38Z</dc:date>
    <item>
      <title>BeeStack: Wakeup other than Keyboard interrupt</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Wakeup-other-than-Keyboard-interrupt/m-p/450114#M21603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using since a long time a system based on MC13213.&lt;/P&gt;&lt;P&gt;It is composed by an "End point" which send periodic data when a BP is pressed (else go to sleep and wakeup with KeyBoard interrupt)&lt;/P&gt;&lt;P&gt;And a coordinator which received data and make action accoding its. (Ack is sent to the end point)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So this system is very simple!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To do this, I started with the exemple MyWirelessAppDemoNonBeaconEndDevice &amp;amp; MyWirelessAppDemoNonBeaconCoordinator&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since last week, I update the system with the last beestack version 3.0.2: BeeKit HCS08 MAC Codebase 2.6.1&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All is ok, but now, the "end point" also Wake up periodically (about 3 or 4 seconds)&lt;/P&gt;&lt;P&gt;It seems to me this is due to a functionnality which I don't remember if exist on my Old stack. This is called "indirect data": Data send by coordinator when end point is in sleeping..&lt;/P&gt;&lt;P&gt;I desactivate all managment of MLME in end point. But may be I forget something?&lt;/P&gt;&lt;P&gt;May be the problem come from other...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then I don't find any way to desactivate a periodic wakeup. (I don't know at this time if it is the Transceiver or the µC timer which Wake up the µC&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;cPWR_DeepSleepMode is set to 1&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 18:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Wakeup-other-than-Keyboard-interrupt/m-p/450114#M21603</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2015-05-20T18:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: BeeStack: Wakeup other than Keyboard interrupt</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Wakeup-other-than-Keyboard-interrupt/m-p/450115#M21604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, I think the µC wakeup&amp;nbsp;&amp;nbsp; because I seen courrent consumption&amp;nbsp; pass from less than 1µA to 8 mA.&lt;/P&gt;&lt;P&gt;In fact, due to Serial link with a computer, current increase periodically I don't know why.&lt;/P&gt;&lt;P&gt;So the µC is keep in sleep.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry:smileyblush:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 05:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Wakeup-other-than-Keyboard-interrupt/m-p/450115#M21604</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2015-05-22T05:10:13Z</dc:date>
    </item>
  </channel>
</rss>