<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S08SG micro reset characteristics in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08SG-micro-reset-characteristics/m-p/448268#M21587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on the S08SG microcontroller. What is the effect on the state of the port pins if the Reset line is held low for a considerable duration of time (For e.g. if it is accidently short circuited to Ground). Also, does the micro keep resetting multiple times for the entire duration when the reset line is pulled to low(as it is a low level triggered reset) or it resets just once when the reset line goes high again?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Nov 2015 15:31:08 GMT</pubDate>
    <dc:creator>pratikp1</dc:creator>
    <dc:date>2015-11-26T15:31:08Z</dc:date>
    <item>
      <title>S08SG micro reset characteristics</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08SG-micro-reset-characteristics/m-p/448268#M21587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on the S08SG microcontroller. What is the effect on the state of the port pins if the Reset line is held low for a considerable duration of time (For e.g. if it is accidently short circuited to Ground). Also, does the micro keep resetting multiple times for the entire duration when the reset line is pulled to low(as it is a low level triggered reset) or it resets just once when the reset line goes high again?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Nov 2015 15:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08SG-micro-reset-characteristics/m-p/448268#M21587</guid>
      <dc:creator>pratikp1</dc:creator>
      <dc:date>2015-11-26T15:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: S08SG micro reset characteristics</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08SG-micro-reset-characteristics/m-p/448269#M21588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The reset line force the MCU pins to the high impedance when pulled low. The MCU will reset only once, when the reset lines goes high.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 13:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08SG-micro-reset-characteristics/m-p/448269#M21588</guid>
      <dc:creator>Stano</dc:creator>
      <dc:date>2015-11-27T13:41:27Z</dc:date>
    </item>
  </channel>
</rss>