<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAN tranceiver problem in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-tranceiver-problem/m-p/427716#M21465</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Iam using freescale DSC controller for automotive application.Using this, I want to use CAN communication. So I used can tranceiver LT1796(&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcds.linear.com%2Fdocs%2Fen%2Fdatasheet%2F1796f.pdf" rel="nofollow" target="_blank"&gt;http://cds.linear.com/docs/en/datasheet/1796f.pdf))&lt;/A&gt; . &lt;/P&gt;&lt;P&gt;But problem is,&amp;nbsp; controller is in 3.3v logic level but LTC tranceiver is in 5v operation.&lt;/P&gt;&lt;P&gt;In S08 controller it works fine with this CAN tranceiver.&lt;/P&gt;&lt;P&gt;Can I use 3.3v controller with 5v CAN tranceiver?&lt;/P&gt;&lt;P&gt;If not please suggest a tranceiver IC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2015 12:15:16 GMT</pubDate>
    <dc:creator>binukannur</dc:creator>
    <dc:date>2015-06-24T12:15:16Z</dc:date>
    <item>
      <title>CAN tranceiver problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-tranceiver-problem/m-p/427716#M21465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Iam using freescale DSC controller for automotive application.Using this, I want to use CAN communication. So I used can tranceiver LT1796(&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcds.linear.com%2Fdocs%2Fen%2Fdatasheet%2F1796f.pdf" rel="nofollow" target="_blank"&gt;http://cds.linear.com/docs/en/datasheet/1796f.pdf))&lt;/A&gt; . &lt;/P&gt;&lt;P&gt;But problem is,&amp;nbsp; controller is in 3.3v logic level but LTC tranceiver is in 5v operation.&lt;/P&gt;&lt;P&gt;In S08 controller it works fine with this CAN tranceiver.&lt;/P&gt;&lt;P&gt;Can I use 3.3v controller with 5v CAN tranceiver?&lt;/P&gt;&lt;P&gt;If not please suggest a tranceiver IC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 12:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-tranceiver-problem/m-p/427716#M21465</guid>
      <dc:creator>binukannur</dc:creator>
      <dc:date>2015-06-24T12:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: CAN tranceiver problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-tranceiver-problem/m-p/427717#M21466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Provided you adhere to the DC Electrical Characteristics mentioned on the datasheet, I do not see a problem using the LT1796 transceiver. &lt;/P&gt;&lt;P style="margin-left: .5in; text-indent: -.5in;"&gt;&lt;/P&gt;&lt;P style="margin-left: .5in; text-indent: -.5in;"&gt;Please be aware of the following information:&lt;/P&gt;&lt;P style="margin-left: .5in; text-indent: -.5in;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="parameteres.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57998iBB01630FBBA7DED8/image-size/large?v=v2&amp;amp;px=999" role="button" title="parameteres.JPG" alt="parameteres.JPG" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;If the microcontroller can supply the TXD signal with the features needed for the LT1796 transceiver, your application should work correctly. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to get more information about the CAN transceivers from Freescale, please refer to the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/application.jsp?code=APLCAN&amp;amp;fsrch=1&amp;amp;sr=3&amp;amp;pageNum=1" title="http://www.freescale.com/webapp/sps/site/application.jsp?code=APLCAN&amp;amp;fsrch=1&amp;amp;sr=3&amp;amp;pageNum=1"&gt;Controller Area Network (CAN)|Freescale&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="can transceiver.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57999iE0A7575B8F37F139/image-size/large?v=v2&amp;amp;px=999" role="button" title="can transceiver.JPG" alt="can transceiver.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information will be useful for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 16:25:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-tranceiver-problem/m-p/427717#M21466</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2015-06-25T16:25:52Z</dc:date>
    </item>
    <item>
      <title>Re: CAN tranceiver problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-tranceiver-problem/m-p/427718#M21467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; It works fine. The problem is in my hardware side. I remove the pullup resister that Iam already did.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Jun 2015 06:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-tranceiver-problem/m-p/427718#M21467</guid>
      <dc:creator>binukannur</dc:creator>
      <dc:date>2015-06-27T06:03:02Z</dc:date>
    </item>
  </channel>
</rss>