<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 mpxy8300 interrupt illegal_bp problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mpxy8300-interrupt-illegal-bp-problem/m-p/419326#M21442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all guys,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently working on a project using MPXY8300 TPMS chip, which is driven by HSC08 core. However I have encountered problem when using interrupts, and I always get ILLEGAL_BP while debugging. I have read several posts but nothing actually helped me. Here is what I have:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;void main(void) { &amp;nbsp; /* This code continously transmit TPMS packets of type BERU RDE012 */ &amp;nbsp;&amp;nbsp; &amp;nbsp; UINT8 i; &amp;nbsp; volatile UINT8 tmp; &amp;nbsp; volatile UINT8 RFRD_data[11]; &amp;nbsp; UINT16 delay=0; &amp;nbsp;&amp;nbsp; &amp;nbsp; /* Set up MCU and set STOP mode. */ &amp;nbsp; __RESET_WATCHDOG(); &amp;nbsp;&amp;nbsp; &amp;nbsp; vfnSetupMCU(); &amp;nbsp; vfnSetSTOPMode(4);&amp;nbsp; &amp;nbsp; vfnSetupRFX(); &amp;nbsp;&amp;nbsp; &amp;nbsp; EnableInterrupts; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; PTADD |= BIT3;&amp;nbsp; // set pin A3 output&amp;nbsp; &amp;nbsp; LED_OFF; &amp;nbsp; LED_ON; &amp;nbsp; LED_OFF; &amp;nbsp; while(1); } &lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;COP is disabled by writing 0x33 in SOPT1 reg.&lt;/P&gt;&lt;P&gt;Interrupt is defined in another file in the following way:&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;#pragma CODE_SEG NON_BANKED void interrupt VectorNumber_Vwuktmr wup_isr(void) {&amp;nbsp;&amp;nbsp; PWUCS0_WUFACK = SET;&amp;nbsp; PWUCS1_PRFACK = SET;&amp;nbsp;&amp;nbsp; LED_ON;&amp;nbsp; LED_OFF; } #pragma CODE_SEG DEFAULT&lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't use any interrupt table (If I understood correctly,that was an old way, but I also tried with linking error that desired segment is already in use ...).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks in advance for your suggestions,&lt;/P&gt;&lt;P&gt;Nemanja Savic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jul 2015 18:04:23 GMT</pubDate>
    <dc:creator>nemanjasavic</dc:creator>
    <dc:date>2015-07-16T18:04:23Z</dc:date>
    <item>
      <title>mpxy8300 interrupt illegal_bp problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mpxy8300-interrupt-illegal-bp-problem/m-p/419326#M21442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all guys,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently working on a project using MPXY8300 TPMS chip, which is driven by HSC08 core. However I have encountered problem when using interrupts, and I always get ILLEGAL_BP while debugging. I have read several posts but nothing actually helped me. Here is what I have:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;void main(void) { &amp;nbsp; /* This code continously transmit TPMS packets of type BERU RDE012 */ &amp;nbsp;&amp;nbsp; &amp;nbsp; UINT8 i; &amp;nbsp; volatile UINT8 tmp; &amp;nbsp; volatile UINT8 RFRD_data[11]; &amp;nbsp; UINT16 delay=0; &amp;nbsp;&amp;nbsp; &amp;nbsp; /* Set up MCU and set STOP mode. */ &amp;nbsp; __RESET_WATCHDOG(); &amp;nbsp;&amp;nbsp; &amp;nbsp; vfnSetupMCU(); &amp;nbsp; vfnSetSTOPMode(4);&amp;nbsp; &amp;nbsp; vfnSetupRFX(); &amp;nbsp;&amp;nbsp; &amp;nbsp; EnableInterrupts; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; PTADD |= BIT3;&amp;nbsp; // set pin A3 output&amp;nbsp; &amp;nbsp; LED_OFF; &amp;nbsp; LED_ON; &amp;nbsp; LED_OFF; &amp;nbsp; while(1); } &lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;COP is disabled by writing 0x33 in SOPT1 reg.&lt;/P&gt;&lt;P&gt;Interrupt is defined in another file in the following way:&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;#pragma CODE_SEG NON_BANKED void interrupt VectorNumber_Vwuktmr wup_isr(void) {&amp;nbsp;&amp;nbsp; PWUCS0_WUFACK = SET;&amp;nbsp; PWUCS1_PRFACK = SET;&amp;nbsp;&amp;nbsp; LED_ON;&amp;nbsp; LED_OFF; } #pragma CODE_SEG DEFAULT&lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't use any interrupt table (If I understood correctly,that was an old way, but I also tried with linking error that desired segment is already in use ...).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks in advance for your suggestions,&lt;/P&gt;&lt;P&gt;Nemanja Savic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2015 18:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mpxy8300-interrupt-illegal-bp-problem/m-p/419326#M21442</guid>
      <dc:creator>nemanjasavic</dc:creator>
      <dc:date>2015-07-16T18:04:23Z</dc:date>
    </item>
  </channel>
</rss>