<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC68HC908GR60A security field values restriction?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908GR60A-security-field-values-restriction/m-p/418452#M21432</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jozef,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No matter what value programmed in memory address 0xFFF6-0xFFFD, the flash will be security after programmed.&lt;/P&gt;&lt;P&gt;For security reason, please do not leave 0xFFF6~0xFFFD to blank.&lt;/P&gt;&lt;P&gt;And there is no restriction on the value be programmed at 0xFFF6~0xFFFD, but you need to know the data that has been programmed for monitor mode entry.&lt;/P&gt;&lt;P&gt;Please see section '19.3.2 Security' of MC68HC908GR16 for further reference!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jul 2015 02:25:54 GMT</pubDate>
    <dc:creator>Rick_Li</dc:creator>
    <dc:date>2015-07-21T02:25:54Z</dc:date>
    <item>
      <title>MC68HC908GR60A security field values restriction?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908GR60A-security-field-values-restriction/m-p/418451#M21431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial,Helvetica,sans-serif; font-size: 10pt;"&gt;Hi, &lt;BR /&gt; &lt;BR /&gt;I am trying to program the address 0xFFF6-FFFD with values 0x00. But after programming and verifying the flash memory the MCU seems to be secured. &lt;BR /&gt;Read values are 0xAF. Is it possible to program all security bytes with 0x00? &lt;BR /&gt;Is there any restriction which value should or should not be at 0xFFF6-FFFD? &lt;BR /&gt;When I program random data at 0xFFF6-FFFD then the verify is OK. &lt;BR /&gt; &lt;BR /&gt;BR, &lt;BR /&gt;Jozef&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2015 06:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908GR60A-security-field-values-restriction/m-p/418451#M21431</guid>
      <dc:creator>guide19</dc:creator>
      <dc:date>2015-07-17T06:51:51Z</dc:date>
    </item>
    <item>
      <title>Re: MC68HC908GR60A security field values restriction?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908GR60A-security-field-values-restriction/m-p/418452#M21432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jozef,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No matter what value programmed in memory address 0xFFF6-0xFFFD, the flash will be security after programmed.&lt;/P&gt;&lt;P&gt;For security reason, please do not leave 0xFFF6~0xFFFD to blank.&lt;/P&gt;&lt;P&gt;And there is no restriction on the value be programmed at 0xFFF6~0xFFFD, but you need to know the data that has been programmed for monitor mode entry.&lt;/P&gt;&lt;P&gt;Please see section '19.3.2 Security' of MC68HC908GR16 for further reference!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 02:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908GR60A-security-field-values-restriction/m-p/418452#M21432</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2015-07-21T02:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: MC68HC908GR60A security field values restriction?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908GR60A-security-field-values-restriction/m-p/418453#M21433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yong Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;No matter what value programmed in memory address 0xFFF6-0xFFFD, the flash will be security after programmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Yes I have the same experience, but for that case it seems that something is not working OK.&lt;/P&gt;&lt;P&gt; I also realized, that when I program security values on 0XFFF6-0xFFFD where minimum 5 from 8 bytes are equal 0x00 (doesn't matter what position they are) than even if I send correct security values at the beginning of entering Monitor mode, I am not able to read the MCU and it looks like the MCU is secured.&lt;/P&gt;&lt;P&gt;When maximum 4 from 8 security bytes are 0x00 than everything works how it should be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have this MCU in your office? is it possible to try program all security fields to 0x00 and test if everything works fine and you can re-read the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Jozef&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 05:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68HC908GR60A-security-field-values-restriction/m-p/418453#M21433</guid>
      <dc:creator>guide19</dc:creator>
      <dc:date>2015-07-21T05:22:49Z</dc:date>
    </item>
  </channel>
</rss>