<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: HCS08 - MC9S08AW60 Output Array</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412632#M21403</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Simon Forster,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no such a type for your array since HCS08 does not support a bit access.&lt;/P&gt;&lt;P&gt;The elements in your array are BITs of a byte register.&lt;/P&gt;&lt;P&gt;In the header file of MC9S08AW60, you will see the port data register are defined as a union and each pin is defined as PTxD_PTxDx. that is to say, the elements in your array has already defined, you can not use it in the array again!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jul 2015 03:31:56 GMT</pubDate>
    <dc:creator>Rick_Li</dc:creator>
    <dc:date>2015-07-15T03:31:56Z</dc:date>
    <item>
      <title>HCS08 - MC9S08AW60 Output Array</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412631#M21402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been working the ARM mBed, but soon found out that I didn't have enough I/O pins and so I went over to the MC9S08AW60.&amp;nbsp; I am trying to use a similar code that I had running on the mBed but have encountered an issue around a 2D array with port values.&amp;nbsp;&amp;nbsp; My issues is I am unsure how what the &amp;lt;type&amp;gt; should be for the array.&amp;nbsp; I have tried multiple things such as int, char etc and I haven't been able to get it to work. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The code I had working on the mBed is:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;DigitalOut ledTable [&lt;/SPAN&gt;&lt;SPAN class="s2"&gt;5&lt;/SPAN&gt;&lt;SPAN class="s1"&gt;][&lt;/SPAN&gt;&lt;SPAN class="s2"&gt;5&lt;/SPAN&gt;&lt;SPAN class="s1"&gt;] =&amp;nbsp; {{(p6), (p11), (p16), (p25), (p30)},{(p7), (p12), (p17), (p24), (p29)},{(p8), (p13), (p18), (p23), (p28)},{(p9), (p14), (p19), (p22), (p27)},{(p10), (p15), (p20), (p21), (p26)}};&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN class="s3"&gt;//defines the ports used on the mBed, table representation of this below&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1" style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="s3"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s3"&gt;In this code I used the &amp;lt;type&amp;gt; for the array as DigitalOut, is there an equivalent on the MC9S08AW60?&amp;nbsp; As for far I have the rewritten the code for the same array to be used on the MC9S08AW60, but as I said I can't find a correct &amp;lt;type&amp;gt; to give the array, any help would be much appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1" style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&amp;lt;type????&amp;gt; ledTable[&lt;/SPAN&gt;&lt;SPAN class="s2"&gt;5&lt;/SPAN&gt;&lt;SPAN class="s1"&gt;][&lt;/SPAN&gt;&lt;SPAN class="s2"&gt;5&lt;/SPAN&gt;&lt;SPAN class="s1"&gt;] ; {&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt; {PTBD_PTBD5, PTBD_PTBD6, PTBD_PTBD7, PTDD_PTDD0, PTDD_PTDD1} ,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt; {PTBD_PTBD0, PTBD_PTBD1, PTBD_PTBD2, PTBD_PTBD3, PTBD_PTBD4} ,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt; {PTED_PTED3, PTED_PTED4, PTED_PTED5, PTED_PTED6, PTED_PTED7} ,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt; {PTAD_PTAD6, PTAD_PTAD7, PTED_PTED0, PTED_PTED1, PTED_PTED2} ,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt; {PTAD_PTAD1, PTAD_PTAD2, PTAD_PTAD3, PTAD_PTAD4, PTAD_PTAD5}&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt; };&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 23:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412631#M21402</guid>
      <dc:creator>spforster13</dc:creator>
      <dc:date>2015-07-14T23:26:23Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 - MC9S08AW60 Output Array</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412632#M21403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Simon Forster,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no such a type for your array since HCS08 does not support a bit access.&lt;/P&gt;&lt;P&gt;The elements in your array are BITs of a byte register.&lt;/P&gt;&lt;P&gt;In the header file of MC9S08AW60, you will see the port data register are defined as a union and each pin is defined as PTxD_PTxDx. that is to say, the elements in your array has already defined, you can not use it in the array again!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 03:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412632#M21403</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2015-07-15T03:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 - MC9S08AW60 Output Array</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412633#M21404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think MCU with addressable bits doesn't exist. Some compilers for Microchip MCU's support bit type and even bit addresses, but MCU still has bits packed into byte registers, and only bytes are addressable.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="s1"&gt;I think DigitalOut is some C++ class in ARM environment, Simon is using. I'm not familiar with S08 CW C++, I guess it is doable as well. But I doubt that using C++ on S08 and other tiny MCU's is the right idea. I would use C for the task like this:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;typedef struct{&lt;BR /&gt;&amp;nbsp; volatile char *&amp;nbsp; adr;&lt;BR /&gt;&amp;nbsp; char mask;&lt;BR /&gt;} led;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;const led ledTable[5][5] = {&lt;BR /&gt; {{&amp;amp;PTBD, PTBD_PTBD5_MASK}, {&amp;amp;PTBD, PTBD_PTBD6_MASK}, {&amp;amp;PTBD, PTBD_PTBD7_MASK}, &lt;BR /&gt;&amp;nbsp; {&amp;amp;PTDD, PTDD_PTDD0_MASK}, {&amp;amp;PTDD, PTDD_PTDD1_MASK}&amp;nbsp; },&lt;/P&gt;&lt;P&gt;{{&amp;amp;PTBD, PTBD_PTBD0_MASK}, {&amp;amp;PTBD, PTBD_PTBD1_MASK}, {&amp;amp;PTBD, PTBD_PTBD2_MASK}, &lt;BR /&gt;&amp;nbsp; {&amp;amp;PTBD, PTBD_PTBD3_MASK}, {&amp;amp;PTBD, PTBD_PTBD4_MASK}} ,&lt;/P&gt;&lt;P&gt;// {PTED_PTED3, PTED_PTED4, PTED_PTED5, PTED_PTED6, PTED_PTED7} ,&lt;/P&gt;&lt;P&gt;// {PTAD_PTAD6, PTAD_PTAD7, PTED_PTED0, PTED_PTED1, PTED_PTED2} ,&lt;/P&gt;&lt;P&gt;// {PTAD_PTAD1, PTAD_PTAD2, PTAD_PTAD3, PTAD_PTAD4, PTAD_PTAD5}&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void SetLed( int i, int j, int value) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(value)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ledTable[i][j].adr |= ledTable[i][j].mask;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ledTable[i][j].adr &amp;amp;= ~ledTable[i][j].mask;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int GetLed( int i, int j) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(*ledTable[i][j].adr &amp;amp; ledTable[i][j].mask)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0;&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 07:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412633#M21404</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2015-07-15T07:38:32Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 - MC9S08AW60 Output Array</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412634#M21405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much Edward,&amp;nbsp; I have now got my program working how I want it with the structure of the table you outlined along with &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;*ledTable[i][j].adr |= ledTable[i][j].mask; and &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;*ledTable[i][j].adr &amp;amp;= ~ledTable[i][j].mask; to turn them off.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 10:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-MC9S08AW60-Output-Array/m-p/412634#M21405</guid>
      <dc:creator>spforster13</dc:creator>
      <dc:date>2015-07-15T10:40:52Z</dc:date>
    </item>
  </channel>
</rss>