<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックDesign Note: To prevent S08PA/PT hung up by multiple short reset signals when POR</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Design-Note-To-prevent-S08PA-PT-hung-up-by-multiple-short-reset/m-p/411442#M21398</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found that S08PA/PT family can be hung up by multiple short reset signals input to reset pin when POR.&lt;/P&gt;&lt;P&gt;To put RC components on reset pin is suggested as what in document.&lt;/P&gt;&lt;P&gt;The hung up issue happens when no RC on reset pin.&lt;/P&gt;&lt;P&gt;The workaround is:&lt;/P&gt;&lt;P&gt;1) To configure reset as a GPIO.&lt;/P&gt;&lt;P&gt;2) To enable internal glitch filter in the beginning of main() as below, the filter clock source must be LPOCLK rather than BUSCLK. It's not a total solution due to MCU could be hung up at some corner conditions:&lt;/P&gt;&lt;P&gt;PORT_IOFLT2_FLTRST = 3;&lt;/P&gt;&lt;P&gt;PORT_FCLKDIV_FLTDIV3 = 7;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120320iE5E5EC6949C641B8/image-size/large?v=v2&amp;amp;px=999" title="24843_24843.png" alt="24843_24843.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31675iC9D9A32AB7D37901/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 May 2015 02:25:09 GMT</pubDate>
    <dc:creator>LaMoris</dc:creator>
    <dc:date>2015-05-08T02:25:09Z</dc:date>
    <item>
      <title>Design Note: To prevent S08PA/PT hung up by multiple short reset signals when POR</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Design-Note-To-prevent-S08PA-PT-hung-up-by-multiple-short-reset/m-p/411442#M21398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found that S08PA/PT family can be hung up by multiple short reset signals input to reset pin when POR.&lt;/P&gt;&lt;P&gt;To put RC components on reset pin is suggested as what in document.&lt;/P&gt;&lt;P&gt;The hung up issue happens when no RC on reset pin.&lt;/P&gt;&lt;P&gt;The workaround is:&lt;/P&gt;&lt;P&gt;1) To configure reset as a GPIO.&lt;/P&gt;&lt;P&gt;2) To enable internal glitch filter in the beginning of main() as below, the filter clock source must be LPOCLK rather than BUSCLK. It's not a total solution due to MCU could be hung up at some corner conditions:&lt;/P&gt;&lt;P&gt;PORT_IOFLT2_FLTRST = 3;&lt;/P&gt;&lt;P&gt;PORT_FCLKDIV_FLTDIV3 = 7;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120320iE5E5EC6949C641B8/image-size/large?v=v2&amp;amp;px=999" title="24843_24843.png" alt="24843_24843.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31675iC9D9A32AB7D37901/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 02:25:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Design-Note-To-prevent-S08PA-PT-hung-up-by-multiple-short-reset/m-p/411442#M21398</guid>
      <dc:creator>LaMoris</dc:creator>
      <dc:date>2015-05-08T02:25:09Z</dc:date>
    </item>
  </channel>
</rss>