<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Port B bit 0 as output on PA4 soic-20 pkg in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409885#M21384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tony&lt;/P&gt;&lt;P&gt;yes, this is correct&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55286iBB32EDBD26E4A942/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Aug 2015 21:01:28 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2015-08-06T21:01:28Z</dc:date>
    <item>
      <title>Port B bit 0 as output on PA4 soic-20 pkg</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409881#M21380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't make it drive a ULN2003 (~170uA).&lt;/P&gt;&lt;P&gt;Tried 2 chips, both same syndrome.&lt;/P&gt;&lt;P&gt;Works fine as input, with pull up or not.&lt;/P&gt;&lt;P&gt;Same circuitry using bits 0-5 as outputs, 1-5 behave fine.&lt;/P&gt;&lt;P&gt;With 15+ years using 68xxx08 chips, I think I found my 1st errata.&lt;/P&gt;&lt;P&gt;Am I missing something here?&amp;nbsp; TNX K.Sargent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2015 12:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409881#M21380</guid>
      <dc:creator>CustomSarge</dc:creator>
      <dc:date>2015-08-04T12:11:37Z</dc:date>
    </item>
    <item>
      <title>Re: Port B bit 0 as output on PA4 soic-20 pkg</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409882#M21381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you sure this is not of those few pins (usually 2) that are either input-only or output-only?&amp;nbsp; PA4 in some MCUs was that case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2015 16:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409882#M21381</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2015-08-04T16:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: Port B bit 0 as output on PA4 soic-20 pkg</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409883#M21382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I scoured the datasheet... no reference.&lt;/P&gt;&lt;P&gt;I'm also 3 for 3... put an soic-20 on a test conversion board.&lt;/P&gt;&lt;P&gt;Put same code (as simple as it gets...) Same Result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS Pins typed as input only "shouldn't" reset the cpu on enough pullup to make them behave as outputs...&lt;/P&gt;&lt;P&gt;I had to remap b3 to b0 (a luxury of this design) and it ... works just fine.&lt;/P&gt;&lt;P&gt;Somebody at Freescale needs to step up and tell me I'm wrong or WHAT...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 01:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409883#M21382</guid>
      <dc:creator>CustomSarge</dc:creator>
      <dc:date>2015-08-05T01:44:30Z</dc:date>
    </item>
    <item>
      <title>Re: Port B bit 0 as output on PA4 soic-20 pkg</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409884#M21383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just read the S08PA4 reference which states "PTB0 provide true open drain when operated as output."&amp;nbsp; Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 13:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409884#M21383</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2015-08-06T13:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: Port B bit 0 as output on PA4 soic-20 pkg</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409885#M21384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tony&lt;/P&gt;&lt;P&gt;yes, this is correct&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55286iBB32EDBD26E4A942/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 21:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409885#M21384</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-08-06T21:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: Port B bit 0 as output on PA4 soic-20 pkg</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409886#M21385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Howdy, Yup, I stand corrected. It's logged in:&lt;/P&gt;&lt;P&gt;Pg 139 of RM&lt;/P&gt;&lt;P&gt;Pg 34 of RM (as copied)&lt;/P&gt;&lt;P&gt;Pg 7 of DS note #4&lt;/P&gt;&lt;P&gt;Pg 27 of DS note #2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was working from the port description section and missed it.&lt;/P&gt;&lt;P&gt;I'd appreciate stuffing a note in the output enable section, at the b0 descriptor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll maintain that when I put enough pullup (1k) to drive the ULN2003,&lt;/P&gt;&lt;P&gt;&amp;nbsp; turning it off (low) reset the processor... odd.&lt;/P&gt;&lt;P&gt;I tried 2.2k, well enough to pull .2mA, but output (as data=1) didn't rise enough.&lt;/P&gt;&lt;P&gt;I saw ~1.5V (Vdd=3.3) when set as output and data=1, not exactly OC behavior,&lt;/P&gt;&lt;P&gt;&amp;nbsp; with nothing connected to pin.&lt;/P&gt;&lt;P&gt;I'm just observing strange stuff, and have no time to do a real proof.&lt;/P&gt;&lt;P&gt;I just remapped b7&amp;lt;-&amp;gt;b0 since my b7 was an input, working fine.&lt;/P&gt;&lt;P&gt;Thanks for the guidance (D+ on my incomplete homework...)&amp;nbsp; K.Sargent&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2015 00:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Port-B-bit-0-as-output-on-PA4-soic-20-pkg/m-p/409886#M21385</guid>
      <dc:creator>CustomSarge</dc:creator>
      <dc:date>2015-08-07T00:10:41Z</dc:date>
    </item>
  </channel>
</rss>