<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: an2295 with JM60, Master does not appear to be relocating interrupt vectors. in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/an2295-with-JM60-Master-does-not-appear-to-be-relocating/m-p/407133#M21362</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The merge tool comes with AN2295SW.&lt;/P&gt;&lt;P&gt;After download AN2295SW from Freescale website (you can search AN295 from Freescale web site and download it) and then extract this software.&lt;/P&gt;&lt;P&gt;Then you will find the merge tool 'win_bisrconv.exe' in folder {AN2295SW}\masters\release\.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This tool can convert the vector for you automatically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jul 2015 05:48:31 GMT</pubDate>
    <dc:creator>Rick_Li</dc:creator>
    <dc:date>2015-07-03T05:48:31Z</dc:date>
    <item>
      <title>an2295 with JM60, Master does not appear to be relocating interrupt vectors.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/an2295-with-JM60-Master-does-not-appear-to-be-relocating/m-p/407132#M21361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to add a bootloader function to a piece of firmware that is already fully functioning and tested. I am using the AN2295 Developer's Serial Bootloader to load load my main application onto my board which uses a JM60 8 bit micro.&amp;nbsp; I have imported and built the bootloader project and was able to program my device with the bootloader firmware.&amp;nbsp; I am able to connect to to the device with the master just fine, but when it looks at my s19 file it gives to following warning:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;WARNING! S19 image will not fit into available memory (at address 0xFFBD)!&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is where it is defining the interrupt vectors of my program, when I go to AutoProgram I get the following:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Memory reading block 0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R 0xFFBD 99%&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Verification failed at block 0, address 0xFFBD, image: [0xFF], MCU: [0xFC]&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Program memory failed.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Memory reading block 0:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R 0xFFBD 99%&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Verification failed at block 0, address 0xFFBD, image: [0xFF], MCU: [0xFC]&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Program memory failed.&lt;/EM&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From what I have read in the application note and in the forums, it looks like the master software is supposed to move these vectors for me, am I wrong in this assumption? Do I need to change some things in the settings files of the project to get this to work properly?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, I can't find the S19 Merge Tool software that is mentioned in section 11 of AN2295 on the Freescale website, can I get a link for this download?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 18:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/an2295-with-JM60-Master-does-not-appear-to-be-relocating/m-p/407132#M21361</guid>
      <dc:creator>dm1001</dc:creator>
      <dc:date>2015-05-28T18:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: an2295 with JM60, Master does not appear to be relocating interrupt vectors.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/an2295-with-JM60-Master-does-not-appear-to-be-relocating/m-p/407133#M21362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The merge tool comes with AN2295SW.&lt;/P&gt;&lt;P&gt;After download AN2295SW from Freescale website (you can search AN295 from Freescale web site and download it) and then extract this software.&lt;/P&gt;&lt;P&gt;Then you will find the merge tool 'win_bisrconv.exe' in folder {AN2295SW}\masters\release\.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This tool can convert the vector for you automatically.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 05:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/an2295-with-JM60-Master-does-not-appear-to-be-relocating/m-p/407133#M21362</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2015-07-03T05:48:31Z</dc:date>
    </item>
  </channel>
</rss>