<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Ethernet</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ethernet/m-p/403218#M21349</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eliezer&lt;/P&gt;&lt;P&gt;I am not sure if I got properly your problem.&lt;/P&gt;&lt;P&gt;You are using the PT60 on your project and you want to add a Ethernet communication to your design.&lt;/P&gt;&lt;P&gt;For this you will add an IC that make the communication between the Ethernet to the S08PT, like a bridge?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that there are ICs that are USB-ethernet bridge but the S08PT does not have USB module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe there are a UART -Ethernet bridge, if this is the case you only need to set the uart at the proper baud rate&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Oct 2015 20:42:41 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2015-10-21T20:42:41Z</dc:date>
    <item>
      <title>Ethernet</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ethernet/m-p/403217#M21348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hello people.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I'm developing an application with PT 60. This application must have Ethernet communication.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Deviso the low cost required by the customer will have to utilisar an IC for Ethernet.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The hardware part of this right, the problem is the Ethernet communication software.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can anyone help me? Thank you.&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 14:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Ethernet/m-p/403217#M21348</guid>
      <dc:creator>eliezeroc</dc:creator>
      <dc:date>2015-10-16T14:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ethernet/m-p/403218#M21349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eliezer&lt;/P&gt;&lt;P&gt;I am not sure if I got properly your problem.&lt;/P&gt;&lt;P&gt;You are using the PT60 on your project and you want to add a Ethernet communication to your design.&lt;/P&gt;&lt;P&gt;For this you will add an IC that make the communication between the Ethernet to the S08PT, like a bridge?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that there are ICs that are USB-ethernet bridge but the S08PT does not have USB module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe there are a UART -Ethernet bridge, if this is the case you only need to set the uart at the proper baud rate&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 20:42:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Ethernet/m-p/403218#M21349</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-10-21T20:42:41Z</dc:date>
    </item>
  </channel>
</rss>