<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Como ler e programar 9S08DZ32 com USBDM?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399552#M21329</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adriano,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You must use either the linker or a third-party tool to generate a binary version of the application. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The most common third-party utility used for converting S-records, which should be correctly generated by the linker if you enable to "Generate S-record" option in the Linker settings panel, to binary images in SREC2BIN.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you can download a copy of it from the following site:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.s-record.com/"&gt;http://www.s-record.com/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 May 2015 01:54:10 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2015-05-05T01:54:10Z</dc:date>
    <item>
      <title>Como ler e programar 9S08DZ32 com USBDM?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399551#M21328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;O software somente reconhece arquivos com extensão .s19 ou .elf, preciso gravar arquivos com extensão .bin, eletrônica embarcada (automotiva)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2015 20:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399551#M21328</guid>
      <dc:creator>adrianomarques</dc:creator>
      <dc:date>2015-05-04T20:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: Como ler e programar 9S08DZ32 com USBDM?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399552#M21329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adriano,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You must use either the linker or a third-party tool to generate a binary version of the application. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The most common third-party utility used for converting S-records, which should be correctly generated by the linker if you enable to "Generate S-record" option in the Linker settings panel, to binary images in SREC2BIN.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you can download a copy of it from the following site:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.s-record.com/"&gt;http://www.s-record.com/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 01:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399552#M21329</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-05-05T01:54:10Z</dc:date>
    </item>
    <item>
      <title>Re: Como ler e programar 9S08DZ32 com USBDM?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399553#M21330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply zhang Jennie!&lt;/P&gt;&lt;P&gt;I can not use the suggested software&lt;/P&gt;&lt;P&gt;I do not have much knowledge in programming&lt;/P&gt;&lt;P&gt;I need to convert a .bin file to .s19&lt;/P&gt;&lt;P&gt;I need to read the file, modify and rewrite the MC9S08DZ32&lt;/P&gt;&lt;P&gt;I downloaded and installed "codewarrior version 6 and 10, &lt;SPAN style="font-size: 13.3333330154419px;"&gt;bin2srec,&amp;nbsp; srec2bin &lt;/SPAN&gt;but do not know use&lt;/P&gt;&lt;P&gt;I need a "step by step" easy to understand&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my skype: chavcar1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 17:48:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399553#M21330</guid>
      <dc:creator>adrianomarques</dc:creator>
      <dc:date>2015-05-05T17:48:09Z</dc:date>
    </item>
    <item>
      <title>Re: Como ler e programar 9S08DZ32 com USBDM?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399554#M21331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adriano,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can also use burner.exe file to covert s19 file to binary file.&lt;/P&gt;&lt;P&gt;Erich blog has one document covered this topic:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2012/09/27/s-record-intel-hex-and-binary-files/" title="http://mcuoneclipse.com/2012/09/27/s-record-intel-hex-and-binary-files/"&gt;http://mcuoneclipse.com/2012/09/27/s-record-intel-hex-and-binary-files/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope this helps!&lt;BR /&gt;Have a great day,&lt;BR /&gt;Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 02:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399554#M21331</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2015-05-06T02:56:45Z</dc:date>
    </item>
    <item>
      <title>Re: Como ler e programar 9S08DZ32 com USBDM?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399555#M21332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Zhang Jun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to convert binary file to S.19.&lt;/P&gt;&lt;P&gt;but I do not believe it solves my problem&lt;/P&gt;&lt;P&gt;I think I'll have to use a compiler&lt;/P&gt;&lt;P&gt;reading binary file should not contain all the necessary data&lt;/P&gt;&lt;P&gt;This microprocessor is shielded from reading and erasure of data, by FPROT&lt;/P&gt;&lt;P&gt;I think the solution is to create a new project and insert the micro&lt;/P&gt;&lt;P&gt;but it would be interesting to preserve the original data of EEPROM and flash, I understand that you can not&lt;/P&gt;&lt;P&gt;USBDM available makes a read only "DOS" without form, I would have to copy and paste the data in a file with extension .s19 (SREC), but still do not know to this process and I do not know if it would work ..&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adriano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 12:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399555#M21332</guid>
      <dc:creator>adrianomarques</dc:creator>
      <dc:date>2015-05-06T12:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: Como ler e programar 9S08DZ32 com USBDM?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399556#M21333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Colleagues here forum can read and program MC9S08DZ32 with USBDM? They know tell me if it really works? &lt;/P&gt;&lt;P style="color: #444444; font-family: Arial, Verdana, sans-serif; font-size: 13.3333330154419px;"&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 14pt;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="gravador-freescale-hcs08-coldfire-v1-coldfire_MLB-O-3226194166_102012.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4933i01C15FAE0C1A02C4/image-size/large?v=v2&amp;amp;px=999" role="button" title="gravador-freescale-hcs08-coldfire-v1-coldfire_MLB-O-3226194166_102012.jpg" alt="gravador-freescale-hcs08-coldfire-v1-coldfire_MLB-O-3226194166_102012.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.usbdm.com.br/" title="http://www.usbdm.com.br/"&gt;gravador freescale USBDM&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 00:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399556#M21333</guid>
      <dc:creator>adrianomarques</dc:creator>
      <dc:date>2015-05-08T00:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: Como ler e programar 9S08DZ32 com USBDM?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399557#M21334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tested this, but only identified a MC9S12DG256B&lt;/P&gt;&lt;P&gt;He did not identify the 9S08DZ32&lt;/P&gt;&lt;P&gt;The TCL Interpreter did not connect&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Bdm-USBDM-OSBDM-8-16-32-programador-emulador-XS128-Freescale.jpg_350x350.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61181iBA53695BF3C3F77A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Bdm-USBDM-OSBDM-8-16-32-programador-emulador-XS128-Freescale.jpg_350x350.jpg" alt="Bdm-USBDM-OSBDM-8-16-32-programador-emulador-XS128-Freescale.jpg_350x350.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 23:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Como-ler-e-programar-9S08DZ32-com-USBDM/m-p/399557#M21334</guid>
      <dc:creator>adrianomarques</dc:creator>
      <dc:date>2015-07-02T23:56:45Z</dc:date>
    </item>
  </channel>
</rss>