<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Emulate ft245 with hcs08 is it possible? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Emulate-ft245-with-hcs08-is-it-possible/m-p/396717#M21309</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! i've an old application that use ft245 for usb connection; i'd like change it with another component, because my costumer report some fault; Can I use an HCS08 device like jb or js family for emultate ftdi device? it's possible use libusb driver instead to ftdi driver and make work again the application or i need to design again also the pc sw application for work with hcs?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jun 2015 13:50:24 GMT</pubDate>
    <dc:creator>elettronicarewo</dc:creator>
    <dc:date>2015-06-12T13:50:24Z</dc:date>
    <item>
      <title>Emulate ft245 with hcs08 is it possible?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Emulate-ft245-with-hcs08-is-it-possible/m-p/396717#M21309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! i've an old application that use ft245 for usb connection; i'd like change it with another component, because my costumer report some fault; Can I use an HCS08 device like jb or js family for emultate ftdi device? it's possible use libusb driver instead to ftdi driver and make work again the application or i need to design again also the pc sw application for work with hcs?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2015 13:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Emulate-ft245-with-hcs08-is-it-possible/m-p/396717#M21309</guid>
      <dc:creator>elettronicarewo</dc:creator>
      <dc:date>2015-06-12T13:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Emulate ft245 with hcs08 is it possible?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Emulate-ft245-with-hcs08-is-it-possible/m-p/396718#M21310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case I recommend the Flexis JM board with SD Card drivers and USB connectivity, DEMOFLEXISJMSD.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37608i0EA4EA38B2E86A90/image-size/large?v=v2&amp;amp;px=999" title="DEMOFLEXISJMSD.jpg" alt="DEMOFLEXISJMSD.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find more information at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMOFLEXISJMSD"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMOFLEXISJMSD&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information will be useful for you.&lt;/P&gt;&lt;P&gt;Have a great day.&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 16:08:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Emulate-ft245-with-hcs08-is-it-possible/m-p/396718#M21310</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2015-06-16T16:08:25Z</dc:date>
    </item>
  </channel>
</rss>