<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: SPI Query</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-Query/m-p/389282#M21264</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Adrian. I cheked the reference manual in MOSI and MISO. I solve the configuration for SPI.&lt;/P&gt;&lt;P&gt;Now i have some code acoording of SPI in &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; single-wire bidirectional mode. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just need testing it, thanks for reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Jan 2015 14:49:37 GMT</pubDate>
    <dc:creator>carlosomarharoc</dc:creator>
    <dc:date>2015-01-08T14:49:37Z</dc:date>
    <item>
      <title>SPI Query</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-Query/m-p/389280#M21262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have some questions&amp;nbsp; about SPI function&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the SPI working in bidirectional mode. ¿Can I send dates to the slaves and can receive dates from slaves?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know if I explained&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I really appreciate your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jan 2015 17:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-Query/m-p/389280#M21262</guid>
      <dc:creator>carlosomarharoc</dc:creator>
      <dc:date>2015-01-06T17:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Query</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-Query/m-p/389281#M21263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, if the SPI module supports single-wire bidirectional mode it works just like the normal SPI mode but using just one pin in master mode and slave mode in this case MOMI for master and SISO for SLAVE. Please refer to the section &lt;STRONG&gt;MOSI — Master Data Out, Slave Data In&lt;/STRONG&gt; and &lt;STRONG&gt;MISO — Master Data In, Slave Data Out&lt;/STRONG&gt; in the reference manual there you can check the information how the SPI lines behave when bidirectional mode is activated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here you can see a table that compares Normal Mode and Bidirectional Mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48992iDF8BA201EFF58B81/image-size/large?v=v2&amp;amp;px=999" title="spi mode 8 bits.jpg" alt="spi mode 8 bits.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 17:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-Query/m-p/389281#M21263</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-01-07T17:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Query</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-Query/m-p/389282#M21264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Adrian. I cheked the reference manual in MOSI and MISO. I solve the configuration for SPI.&lt;/P&gt;&lt;P&gt;Now i have some code acoording of SPI in &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; single-wire bidirectional mode. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just need testing it, thanks for reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 14:49:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-Query/m-p/389282#M21264</guid>
      <dc:creator>carlosomarharoc</dc:creator>
      <dc:date>2015-01-08T14:49:37Z</dc:date>
    </item>
  </channel>
</rss>