<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC Vrefl benefit in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-Vrefl-benefit/m-p/385232#M21239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P lang="en-US"&gt;Hallo,&lt;/P&gt;&lt;P lang="en-US"&gt;I use the MC9S08LL16 device and the ADC. There are few pins associated with ADC: Vdda, Vssa, Vrefh, Vrefl and other. The Vrefl is usually tied to Vssa. I would like to know, what is it good for to have separated the Vrefl pin. Can its voltage level be externally 'shifted'? For example with voltage reference to 1.2V?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Jan 2015 19:00:27 GMT</pubDate>
    <dc:creator>gam01hr</dc:creator>
    <dc:date>2015-01-04T19:00:27Z</dc:date>
    <item>
      <title>ADC Vrefl benefit</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-Vrefl-benefit/m-p/385232#M21239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P lang="en-US"&gt;Hallo,&lt;/P&gt;&lt;P lang="en-US"&gt;I use the MC9S08LL16 device and the ADC. There are few pins associated with ADC: Vdda, Vssa, Vrefh, Vrefl and other. The Vrefl is usually tied to Vssa. I would like to know, what is it good for to have separated the Vrefl pin. Can its voltage level be externally 'shifted'? For example with voltage reference to 1.2V?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 19:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-Vrefl-benefit/m-p/385232#M21239</guid>
      <dc:creator>gam01hr</dc:creator>
      <dc:date>2015-01-04T19:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Vrefl benefit</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-Vrefl-benefit/m-p/385233#M21240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin Gazda,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As mentioned in the reference manual, Vrefh is the high reference voltage for the converter. In some package, Vrefh is connected internally to Vddad.&lt;/P&gt;&lt;P&gt;If externally available, Vrefh may be conected to the same potential as Vddad or&lt;/P&gt;&lt;P&gt;MAY BE DRIVEN BY AN EXTERNAL SOURCE BETWEEN THE MIN Vddad AND THE Vddad POTENTIAL. (page 149 of the below document)&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LL16RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LL16RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LL16RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;As in Characteristics,the Min of Vrefh is 1.8v. (p36 of below document)&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S08LL16.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S08LL16.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S08LL16.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=F…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So, the Vrefh can be from 1.8v to Vddad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2015 03:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-Vrefl-benefit/m-p/385233#M21240</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2015-02-04T03:35:18Z</dc:date>
    </item>
  </channel>
</rss>