<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic EEProm S08PT16 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/EEProm-S08PT16/m-p/384860#M21238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question about the code position for read/write eeprom.&lt;/P&gt;&lt;P&gt;In such cases I have to run the code from RAM ?&lt;/P&gt;&lt;P&gt;I have read the datasheet (Table4-18) and AN4570, but remain a doubt :&lt;/P&gt;&lt;P&gt;When the code is mormally execute in flash, can i read the eeprom value ?&lt;/P&gt;&lt;P&gt;The Program flash Read is considerated also when the code in flash is executed ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120056iBEBAEF846174DB95/image-size/large?v=v2&amp;amp;px=999" title="17153_17153.png" alt="17153_17153.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47755i08C3A1FDEDF10D08/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Dec 2014 08:08:05 GMT</pubDate>
    <dc:creator>IlConte</dc:creator>
    <dc:date>2014-12-02T08:08:05Z</dc:date>
    <item>
      <title>EEProm S08PT16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/EEProm-S08PT16/m-p/384860#M21238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question about the code position for read/write eeprom.&lt;/P&gt;&lt;P&gt;In such cases I have to run the code from RAM ?&lt;/P&gt;&lt;P&gt;I have read the datasheet (Table4-18) and AN4570, but remain a doubt :&lt;/P&gt;&lt;P&gt;When the code is mormally execute in flash, can i read the eeprom value ?&lt;/P&gt;&lt;P&gt;The Program flash Read is considerated also when the code in flash is executed ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120056iBEBAEF846174DB95/image-size/large?v=v2&amp;amp;px=999" title="17153_17153.png" alt="17153_17153.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47755i08C3A1FDEDF10D08/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 08:08:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/EEProm-S08PT16/m-p/384860#M21238</guid>
      <dc:creator>IlConte</dc:creator>
      <dc:date>2014-12-02T08:08:05Z</dc:date>
    </item>
  </channel>
</rss>