<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピックcan ACK package make a interrupt in MC9S08JM60 USB?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/can-ACK-package-make-a-interrupt-in-MC9S08JM60-USB/m-p/367070#M21172</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi everyone,&lt;/P&gt;&lt;P&gt;I'm using USB module of Mc9S08JM60 .I have two questions.&lt;/P&gt;&lt;P&gt;1, if Host send an ACK package,does device make a interrupt ? &lt;/P&gt;&lt;P&gt;2, How to send an ACK package to host in MC9S08JM60?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Jan 2015 02:09:09 GMT</pubDate>
    <dc:creator>wangbaode</dc:creator>
    <dc:date>2015-01-22T02:09:09Z</dc:date>
    <item>
      <title>can ACK package make a interrupt in MC9S08JM60 USB?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/can-ACK-package-make-a-interrupt-in-MC9S08JM60-USB/m-p/367070#M21172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi everyone,&lt;/P&gt;&lt;P&gt;I'm using USB module of Mc9S08JM60 .I have two questions.&lt;/P&gt;&lt;P&gt;1, if Host send an ACK package,does device make a interrupt ? &lt;/P&gt;&lt;P&gt;2, How to send an ACK package to host in MC9S08JM60?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 02:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/can-ACK-package-make-a-interrupt-in-MC9S08JM60-USB/m-p/367070#M21172</guid>
      <dc:creator>wangbaode</dc:creator>
      <dc:date>2015-01-22T02:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: can ACK package make a interrupt in MC9S08JM60 USB?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/can-ACK-package-make-a-interrupt-in-MC9S08JM60-USB/m-p/367071#M21173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wang&lt;/P&gt;&lt;P&gt;I found that you have asked here, I know that you already sold the problem, but I want to document it, so here is my answer&lt;/P&gt;&lt;P&gt;The &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;ACK&lt;/STRONG&gt;&lt;/SPAN&gt; is handled by SIE of &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;USB&lt;/STRONG&gt;&lt;/SPAN&gt; and it does not need the intervention of firmware.&lt;/P&gt;&lt;P&gt;Bit TOKDNEF in Interrupt Status Register(INTSTAT) will be set when the current transaction is completed.&lt;/P&gt;&lt;P&gt;And an interrupt is generated if TOKDNE is set. Then the firmware can read the STAT register to determine the endpoint and BD information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2015 20:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/can-ACK-package-make-a-interrupt-in-MC9S08JM60-USB/m-p/367071#M21173</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-02-04T20:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: can ACK package make a interrupt in MC9S08JM60 USB?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/can-ACK-package-make-a-interrupt-in-MC9S08JM60-USB/m-p/367072#M21174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vicente,&lt;/P&gt;&lt;P&gt;Thank you . According to the document, It's not a problem for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Feb 2015 02:02:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/can-ACK-package-make-a-interrupt-in-MC9S08JM60-USB/m-p/367072#M21174</guid>
      <dc:creator>wangbaode</dc:creator>
      <dc:date>2015-02-05T02:02:47Z</dc:date>
    </item>
  </channel>
</rss>