<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Sending data to HCS08</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Sending-data-to-HCS08/m-p/362752#M21151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How are you sending values from the file?&lt;/P&gt;&lt;P&gt;Since it is coming in device manager (hopefully as a CDC serial port), you can verify your SCI code using teraterm/hyperterm. &lt;/P&gt;&lt;P&gt;I hope you are able to flash the code using CodeWarrior.&lt;/P&gt;&lt;P&gt;Send/receive data from/to the MCU using terminal. This will verify your setup and then you can work on sending data from the file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this post helps you, kindly mark it as correct/helpful answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Arpita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2014 11:34:30 GMT</pubDate>
    <dc:creator>arpitaagarwal-b</dc:creator>
    <dc:date>2014-10-07T11:34:30Z</dc:date>
    <item>
      <title>Sending data to HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Sending-data-to-HCS08/m-p/362751#M21150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bit of a newbie at this, I've spent a few years with the HCS08 MCU but I'm having troubles setting it up so I can constantly send values to it via a file on the PC that is updated every second. I assume this would be done via a serial interface, but the cable I've been provided with is a simple USB-Serial connector. I've tried using this cable and it isn't being detected by CodeWarrior, but shows up in device manager. The demoboard I'm using is the DEMO9S08AW60E&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any help you can provide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 10:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Sending-data-to-HCS08/m-p/362751#M21150</guid>
      <dc:creator>robinnelis</dc:creator>
      <dc:date>2014-10-02T10:46:54Z</dc:date>
    </item>
    <item>
      <title>Re: Sending data to HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Sending-data-to-HCS08/m-p/362752#M21151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How are you sending values from the file?&lt;/P&gt;&lt;P&gt;Since it is coming in device manager (hopefully as a CDC serial port), you can verify your SCI code using teraterm/hyperterm. &lt;/P&gt;&lt;P&gt;I hope you are able to flash the code using CodeWarrior.&lt;/P&gt;&lt;P&gt;Send/receive data from/to the MCU using terminal. This will verify your setup and then you can work on sending data from the file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this post helps you, kindly mark it as correct/helpful answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Arpita&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 11:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Sending-data-to-HCS08/m-p/362752#M21151</guid>
      <dc:creator>arpitaagarwal-b</dc:creator>
      <dc:date>2014-10-07T11:34:30Z</dc:date>
    </item>
  </channel>
</rss>