<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC9S08DZ60AMLH I2C issue</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60AMLH-I2C-issue/m-p/345802#M21084</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find attached to this response an IIC sample code for your device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend testing the mentioned code in order to check if the IIC module is still working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In that way we can be sure if the code or the hardware is the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day. :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Feb 2015 17:33:56 GMT</pubDate>
    <dc:creator>david_diaz</dc:creator>
    <dc:date>2015-02-11T17:33:56Z</dc:date>
    <item>
      <title>MC9S08DZ60AMLH I2C issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60AMLH-I2C-issue/m-p/345801#M21083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;I'm developing the IIC driver for the MC9S08DZ60AMLH processor.&amp;nbsp; At first it was working, then suddenly it stopped.&amp;nbsp; I found a bad solder joint and repaired it, but it still does not work.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whenever I set the MST bit, it immediately clears!&amp;nbsp; The unit never enters master mode - it never sends any data out.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've searched all the datasheets I can find, nothing mentions this as an issue.&amp;nbsp; They all simply say "set the MST bit to enter into master mode and create an IIC START".&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To test the lines I've set the GPIO to output on the same lines and have had no problem making the lines go high and low.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also switched to the other pins (you can use two different sets of pins) and tried it there.&amp;nbsp; Same results.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas?&amp;nbsp; Could the IIC module be damaged?&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Dec 2014 01:25:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60AMLH-I2C-issue/m-p/345801#M21083</guid>
      <dc:creator>Chicago1984</dc:creator>
      <dc:date>2014-12-12T01:25:12Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60AMLH I2C issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60AMLH-I2C-issue/m-p/345802#M21084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find attached to this response an IIC sample code for your device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend testing the mentioned code in order to check if the IIC module is still working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In that way we can be sure if the code or the hardware is the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day. :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 17:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60AMLH-I2C-issue/m-p/345802#M21084</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2015-02-11T17:33:56Z</dc:date>
    </item>
  </channel>
</rss>