<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 pullup on MISO</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/pullup-on-MISO/m-p/326259#M21001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, I have S08PT16&lt;/P&gt;&lt;P&gt;I use the SPI module configured as a master.&lt;/P&gt;&lt;P&gt;The SPI module can be not present and i need to use the same software.&lt;/P&gt;&lt;P&gt;My question is: the MISO (PTB4) have tge pull-up ?&lt;/P&gt;&lt;P&gt;Can i configure the PORT_PTBPE at 1 if is enabled the SPI module ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jan 2015 08:03:42 GMT</pubDate>
    <dc:creator>IlConte</dc:creator>
    <dc:date>2015-01-28T08:03:42Z</dc:date>
    <item>
      <title>pullup on MISO</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/pullup-on-MISO/m-p/326259#M21001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, I have S08PT16&lt;/P&gt;&lt;P&gt;I use the SPI module configured as a master.&lt;/P&gt;&lt;P&gt;The SPI module can be not present and i need to use the same software.&lt;/P&gt;&lt;P&gt;My question is: the MISO (PTB4) have tge pull-up ?&lt;/P&gt;&lt;P&gt;Can i configure the PORT_PTBPE at 1 if is enabled the SPI module ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jan 2015 08:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/pullup-on-MISO/m-p/326259#M21001</guid>
      <dc:creator>IlConte</dc:creator>
      <dc:date>2015-01-28T08:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: pullup on MISO</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/pullup-on-MISO/m-p/326260#M21002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefano&lt;/P&gt;&lt;P&gt;If you configure the Pin as input you can set the pullup enable, but if you configure the pin as SPI (MISO in this case) the internal pullup are disable&lt;/P&gt;&lt;P&gt;I hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Feb 2015 22:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/pullup-on-MISO/m-p/326260#M21002</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-02-04T22:18:16Z</dc:date>
    </item>
  </channel>
</rss>