<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: FreeRTOS JM60 &amp; Bootloader</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129670#M2069</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I created the task2 in to the task1, in the MyTask&lt;/P&gt;&lt;P&gt;see&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;static portTASK_FUNCTION(MyTask, pvParameters) {  (void)pvParameters; /* parameter not used */  FRTOS1_xTaskCreate(MyTask2,    (signed portCHAR *)"mytask2",    configMINIMAL_STACK_SIZE,    (void *)NULL,    1,    (xTaskHandle*)NULL);      for(;;) {   Bit1_NegVal();    //Term1_SendStr("Envio de tarea 1\r");    FRTOS1_vTaskDelay(300/portTICK_RATE_MS);  }}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I try to create the task in the function RTOS_Start() and &lt;SPAN class="short_text"&gt;&lt;SPAN&gt;and yet it does not work, like this&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text"&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="short_text"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;/** ###################################################################**     Filename  : ProcessorExpert.c**     Project   : ProcessorExpert**     Processor : MCF51QE128CLH**     Version   : Driver 01.00**     Compiler  : CodeWarrior ColdFireV1 C Compiler**     Date/Time : 03/07/2010, 10:58 p.m.**     Abstract  :**         Main module.**         This module contains user's application code.**     Settings  :**     Contents  :**         No public methods**** ###################################################################*//* MODULE ProcessorExpert *//* Including needed modules to compile this module/procedure */#include "Cpu.h"#include "Events.h"/* Include shared modules, which are used for whole project */#include "FRTOS1.h"#include "RTOSSWI1.h"#include "RTOSTMR1.h"#include "Term1.h"#include "Inhr2.h"#include "Bit1.h"#include "Bit2.h"#include "PE_Types.h"#include "PE_Error.h"#include "PE_Const.h"#include "IO_Map.h"static portTASK_FUNCTION(MyTask2,pvParameters){  (void)pvParameters; for(;;){  Bit2_NegVal();  //Term1_SendStr("Envio de tarea 2\r");      FRTOS1_vTaskDelay(500/portTICK_RATE_MS);    }}/* User includes (#include below this line is not maintained by Processor Expert) */static portTASK_FUNCTION(MyTask, pvParameters) {  (void)pvParameters; /* parameter not used */      for(;;) {   Bit1_NegVal();    //Term1_SendStr("Envio de tarea 1\r");    FRTOS1_vTaskDelay(300/portTICK_RATE_MS);  }}static void RTOS_Start(void) {  if (FRTOS1_xTaskCreate(      MyTask,  /* pointer to the task */      (signed portCHAR *)"MyTask", /* task name for kernel awareness debugging */      configMINIMAL_STACK_SIZE, /* task stack size */      (void*)NULL, /* optional task startup argument */      1,  /* initial priority */      (xTaskHandle*)NULL /* optional task handle to create */    )!=pdPASS)  {   //Term1_SendStr("Error1\r");  for(;;){}  }    FRTOS1_xTaskCreate(MyTask2,      (signed portCHAR *)"mytask2",      configMINIMAL_STACK_SIZE,      (void *)NULL,      1,      (xTaskHandle*)NULL);              FRTOS1_vTaskStartScheduler();}void main(void){  /* Write your local variable definition here */  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/  PE_low_level_init();  /*** End of Processor Expert internal initialization.                    ***/     /* Write your code here */  /* For example: for(;;) { } */  RTOS_Start();    /*** Don't write any code pass this line, or it will be deleted during code generation. ***/  /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/  for(;;){}  /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***//* END ProcessorExpert *//*** ###################################################################****     This file was created by Processor Expert 4.00 Beta [04.40]**     for the Freescale ColdFireV1 series of microcontrollers.**** ###################################################################*/&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How much task do you think I could created with 8kb of ram??? I dont know why dont works, because is a simple example, best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jul 2010 20:38:19 GMT</pubDate>
    <dc:creator>brauliochi_thin</dc:creator>
    <dc:date>2010-07-07T20:38:19Z</dc:date>
    <item>
      <title>FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129632#M2031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I've ported FreeRTOS to HCS08, and the project targets the SARD and EVB boards. I'm working on making SMAC compatible with this project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Steps&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Download and install FreeRTOS 3.2.4: &lt;/SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freertos.org%2F" rel="nofollow" target="_blank"&gt;FreeRTOS&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Download the attached zip file&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. Unpack it into a temporary directory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4. Following the FreeRTOS directory structure, move the sub-folders into their correct places.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5. Open the RTOSDemo.mcp project in CW 3.1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;6. Deploy to a Freescale SARD or EVB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Ffiles%2Fcommunity_files%2F8BITCOMM%2FFreeRTOS-3.2.4-HCS08_Files.zip" rel="nofollow" target="_blank"&gt;FreeRTOS-3.2.4-HCS08_Files.zip&lt;/A&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by dkindler on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-20&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;02:33 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Mar 2006 05:17:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129632#M2031</guid>
      <dc:creator>jeffw</dc:creator>
      <dc:date>2006-03-18T05:17:06Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129633#M2032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, Jeff:&lt;BR /&gt;&lt;BR /&gt;Will this port run on the HC08 (non-S) as well?&lt;BR /&gt;&lt;BR /&gt;I don't see why not, but I'm not aware of all of the differences. I haven't used an HCS08 part yet, outside of the ZigBee kit (which we dumped).&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Mar 2006 06:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129633#M2032</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-03-18T06:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129634#M2033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The project uses the Processor Expert, so it is pretty easy to port to any MCU supported by that tool. (Yes, PE is good and bad - I know.)&lt;BR /&gt;&lt;BR /&gt;Wouldn't it be cool to have GCC for HCS08? (And Eclispe and an Eclipse BDM plugin.) Any takers?!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Mar 2006 07:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129634#M2033</guid>
      <dc:creator>jeffw</dc:creator>
      <dc:date>2006-03-18T07:19:07Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129635#M2034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;jeffw wrote:&lt;BR /&gt;Wouldn't it be cool to have GCC for HCS08? (And Eclispe and an Eclipse BDM plugin.) Any takers?!&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;I'll take it in a snap... The hard part would be to provide it :smileywink:&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Mar 2006 23:44:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129635#M2034</guid>
      <dc:creator>imajeff</dc:creator>
      <dc:date>2006-03-21T23:44:56Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129636#M2035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;I have a version of FreeRTOS for both the HC08 and S08. For the HC08 you just have to be careful on the ASM code that makes the context switch since that can be optimized using S08 instructions. Other than that, the code is very similar. Let me know if you are interested I can post it here.&lt;/P&gt;&lt;P&gt;RT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2006 06:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129636#M2035</guid>
      <dc:creator>Trenado</dc:creator>
      <dc:date>2006-03-24T06:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129637#M2036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Dear RT:&lt;/P&gt;&lt;P&gt;I'm interested in your FreeRTOS for HC08.&amp;nbsp; I'm currently&amp;nbsp;working on a project with the MC68HC908GP32 and would like to review your FreeRTOS for HC08 in order to consider using it on this chip.&amp;nbsp; Could you please post your FreeRTOS for HC08?&amp;nbsp; Thank you very much.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Miguel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2006 15:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129637#M2036</guid>
      <dc:creator>mcolina_aimme_e</dc:creator>
      <dc:date>2006-03-30T15:52:57Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129638#M2037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I just sent you a copy of the RTOS to your personal email.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Please let me know if you have any questions or comments.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;RT&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2006 00:34:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129638#M2037</guid>
      <dc:creator>Trenado</dc:creator>
      <dc:date>2006-04-12T00:34:11Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129639#M2038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Dear RT,&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Miguel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2006 01:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129639#M2038</guid>
      <dc:creator>mcolina_aimme_e</dc:creator>
      <dc:date>2006-04-12T01:20:27Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129640#M2039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;RT,&lt;BR /&gt;&lt;BR /&gt;You could also submit a version of the RTOS to the "8-Bit Microcontroller Community".&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Apr 2006 05:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129640#M2039</guid>
      <dc:creator>imajeff</dc:creator>
      <dc:date>2006-04-21T05:51:38Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129641#M2040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;I was wondering if you had ever posted the HC08 version of this RTOS on the forum? The link states it is for the HCS08. Are they the same?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2006 04:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129641#M2040</guid>
      <dc:creator>bespenschied</dc:creator>
      <dc:date>2006-06-07T04:20:13Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129642#M2041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Jeffw. &lt;BR /&gt;Could you send me the RTOS for HC08 or give me a link to download this file, I'm working in this kind of microcontrollers in CW5 and I'm very interesting in this topic, but I don't have information about it, &lt;BR /&gt;Thanks a lot.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2006 05:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129642#M2041</guid>
      <dc:creator>erooll</dc:creator>
      <dc:date>2006-07-25T05:25:38Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129643#M2042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Dear everybody&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Could anybody tell me how to port the FreeRTOS on HCS08 to HC08 (GZ60)?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;Khoa&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Aug 2006 15:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129643#M2042</guid>
      <dc:creator>tranvkhoa</dc:creator>
      <dc:date>2006-08-08T15:52:48Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129644#M2043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have problems compiling FreeRTOS. I followed the instructions, but when I try to compile, I get this error 10 times:&lt;BR /&gt;&lt;BR /&gt;"Error : C2450: Expected: ; "&lt;BR /&gt;&lt;BR /&gt;for this line in portable.h:&lt;BR /&gt;&lt;BR /&gt;"portSTACK_TYPE *pxPortInitialiseStack( portSTACK_TYPE *pxTopOfStack, pdTASK_CODE pxCode, void *pvParameters ); "&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;My CodeWarrior version is 5.7.0 and it converts automatically CW 3.1 projects to newer version. Maybe this is the reason for the problem??&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 16:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129644#M2043</guid>
      <dc:creator>arskii</dc:creator>
      <dc:date>2006-08-14T16:13:55Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129645#M2044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Maybe it's because your CW is special edition. If so, you should buy the pro edition. Do you have FreeRTOS for HCS08 or HC08? If you have the one for HC08, please send to me at &lt;A href="mailto:tranvankhoa@gmail.com" rel="nofollow" target="_blank"&gt;tranvankhoa@gmail.com&lt;/A&gt;. Thanks.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 16:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129645#M2044</guid>
      <dc:creator>tranvkhoa</dc:creator>
      <dc:date>2006-08-14T16:52:56Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129646#M2045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have CW Standard Edition and FreeRTOS for HCS08.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 17:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129646#M2045</guid>
      <dc:creator>arskii</dc:creator>
      <dc:date>2006-08-14T17:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129647#M2046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Is there any message related to license limitation error?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 17:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129647#M2046</guid>
      <dc:creator>tranvkhoa</dc:creator>
      <dc:date>2006-08-14T17:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129648#M2047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;No licence errors. Only that one error 11 times, not 10 as I told before..&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Aug 2006 17:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129648#M2047</guid>
      <dc:creator>arskii</dc:creator>
      <dc:date>2006-08-14T17:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129649#M2048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I am just curious if anyone has gotten the Free RTOS for the HC08 yet? I have seen several posts asking about it but have not seen any posts telling where it is. Anyone Know????&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Sep 2006 11:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129649#M2048</guid>
      <dc:creator>bespenschied</dc:creator>
      <dc:date>2006-09-02T11:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129650#M2049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Dear bespenschied:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Back in april of this year I got a response&amp;nbsp;from&amp;nbsp;Rene Trenado regarding FreeRTOS.&amp;nbsp; He kindly offered me a ZIP file containing&amp;nbsp;FreeRTOS for the HCS08 together with&amp;nbsp;a set of&amp;nbsp;instructions regarding its use.&amp;nbsp; The following message contains these instructions.&amp;nbsp; The&amp;nbsp;ZIP file has been attached to this e-mail.&amp;nbsp; If you have any questions regarding FreeRTOS please refer them to Rene Trenado at&amp;nbsp;&lt;A href="mailto:rene.trenado@embeddia.com" rel="nofollow" target="_blank"&gt;rene.trenado@embeddia.com&lt;/A&gt;&amp;nbsp;as I&amp;nbsp;am not well versed in FreeRTOS.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Best regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Miguel&lt;/DIV&gt;&lt;DIV&gt;2006-09-04&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;please reply to: &lt;A href="mailto:miguel.colina.de.vivero@ieee.org" rel="nofollow" target="_blank"&gt;miguel.colina.de.vivero@ieee.org&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;-----Mensaje original-----&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;De: Rene Trenado [mailto:rene.trenado@embeddia.com]&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Enviado el: sábado, 08 de abril de 2006 2:28&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Para: mcolina@aimme.es&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Asunto: Re: FreeRTOS on HC(S)08&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hi,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Sorry for the late response. Here is the CW project that implements FreeRTOS to the HC08 / S08. The project was meant to be used for a S08 GB60/GT60 board with an 32kHz xtal. Please disregard the initialization of PORTF and the ICG on main.c&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The sample application just creates two tasks (plus the IDLE task used by the RTOS). Each of them go to "sleep" at a different frequency. This is the simplest example I could think of (I have others of course).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;To use the code I am sending to you just cut and past the FreeRTOS folder and GT60 HAL under sources of your project root folder. Rename the GT60 HAL folder to GP32 or whatever and provide your own TickTimer.h and TickTimer.c files (the Timer used by the RTOS to generate the tick interrupts). You just have to provide the following timer functions:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;TickTimer_SetFreqHz( configTICK_RATE_HZ );&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;TickTimer_Enable();&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;which are called by port.c by the way...&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;If you have any questions or comments please let me know.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Saludos y que estes bien&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;(tambien hablo castellano)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Rene Trenado&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/2709_freertos_hcs08_version_1_0.zip" rel="nofollow" target="_self"&gt;FreeRTOS_HC(S)08_Version_1.0.zip&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-10-27&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;12:32 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2006 14:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129650#M2049</guid>
      <dc:creator>mcolina_aimme_e</dc:creator>
      <dc:date>2006-09-04T14:27:21Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS on HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129651#M2050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Miguel,&lt;BR /&gt;&lt;BR /&gt;Thanks for the reply and the files. I used to use an RTOS on the 6811 and it was a good way to handle several programs I needed.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2006 11:43:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FreeRTOS-on-HCS08/m-p/129651#M2050</guid>
      <dc:creator>bespenschied</dc:creator>
      <dc:date>2006-09-06T11:43:37Z</dc:date>
    </item>
  </channel>
</rss>