<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックFlextimer PWM sync between 2 Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flextimer-PWM-sync-between-2-Microcontrollers/m-p/306103#M20678</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to use external trigger to synchronise a FTMxCHn and FTMxCHn+1 with another Microcontroller running the same frequency PWM?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The situation is like this&lt;/P&gt;&lt;P&gt;I have a Flextimer running 4 channels (each pair is complementary-combined) on MCU1&lt;/P&gt;&lt;P&gt;I have the same situation in MCU2.&lt;/P&gt;&lt;P&gt;I require the Flextimer in MCU1 to be run as slave to MCU2, being triggered by FTMxCHn out of MCU2 in MODE1&lt;/P&gt;&lt;P&gt;and self triggered (Software triggered in MODE2)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone share an idea how this can be achieved? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Apr 2014 06:14:15 GMT</pubDate>
    <dc:creator>abicash</dc:creator>
    <dc:date>2014-04-29T06:14:15Z</dc:date>
    <item>
      <title>Flextimer PWM sync between 2 Microcontrollers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flextimer-PWM-sync-between-2-Microcontrollers/m-p/306103#M20678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to use external trigger to synchronise a FTMxCHn and FTMxCHn+1 with another Microcontroller running the same frequency PWM?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The situation is like this&lt;/P&gt;&lt;P&gt;I have a Flextimer running 4 channels (each pair is complementary-combined) on MCU1&lt;/P&gt;&lt;P&gt;I have the same situation in MCU2.&lt;/P&gt;&lt;P&gt;I require the Flextimer in MCU1 to be run as slave to MCU2, being triggered by FTMxCHn out of MCU2 in MODE1&lt;/P&gt;&lt;P&gt;and self triggered (Software triggered in MODE2)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone share an idea how this can be achieved? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2014 06:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Flextimer-PWM-sync-between-2-Microcontrollers/m-p/306103#M20678</guid>
      <dc:creator>abicash</dc:creator>
      <dc:date>2014-04-29T06:14:15Z</dc:date>
    </item>
  </channel>
</rss>