<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックUsing BDM in Stop  mode</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286735#M20394</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt; I am using your 9s08sh16 controller for my project. I am also using the stop3 mode of operation&amp;nbsp;&amp;nbsp; I have&amp;nbsp; the&amp;nbsp; P&amp;amp;E BDM USB Multilink interface to attach with the controller.In order to use the BDM in the stop&amp;nbsp; mode I need to set the ENBDM bit but this bit is only accessible&amp;nbsp; by the BDM device.&lt;BR /&gt; My problem is that I can not locate a command in the Hiiwave software to enable the ENBDM bit of BDCSCR&amp;nbsp; register&amp;nbsp; .&lt;BR /&gt; &lt;BR /&gt; Nasim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jun 2013 11:47:49 GMT</pubDate>
    <dc:creator>nasimimtiaz</dc:creator>
    <dc:date>2013-06-11T11:47:49Z</dc:date>
    <item>
      <title>Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286735#M20394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt; I am using your 9s08sh16 controller for my project. I am also using the stop3 mode of operation&amp;nbsp;&amp;nbsp; I have&amp;nbsp; the&amp;nbsp; P&amp;amp;E BDM USB Multilink interface to attach with the controller.In order to use the BDM in the stop&amp;nbsp; mode I need to set the ENBDM bit but this bit is only accessible&amp;nbsp; by the BDM device.&lt;BR /&gt; My problem is that I can not locate a command in the Hiiwave software to enable the ENBDM bit of BDCSCR&amp;nbsp; register&amp;nbsp; .&lt;BR /&gt; &lt;BR /&gt; Nasim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2013 11:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286735#M20394</guid>
      <dc:creator>nasimimtiaz</dc:creator>
      <dc:date>2013-06-11T11:47:49Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286736#M20395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nasimimtiaz, you needn't to do that, debugger will set it automatically.&lt;/P&gt;&lt;P&gt;Typically, this bit is written to 1 by the debug host shortly&lt;/P&gt;&lt;P&gt;after the beginning of a debug session or whenever the debug host resets the target and remains 1 until a normal&lt;/P&gt;&lt;P&gt;reset clears it.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2013 02:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286736#M20395</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-06-18T02:46:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286737#M20396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Weiping&lt;/P&gt;&lt;P&gt;If the ENBDM bit is set then why am I not able to use the BDM debugger in stop mode? As soon as the processor goes in stop the link is&amp;nbsp; lost and I have to do a power cycle to reestablish the link&lt;/P&gt;&lt;P&gt;Nasim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 06:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286737#M20396</guid>
      <dc:creator>nasimimtiaz</dc:creator>
      <dc:date>2013-06-20T06:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286738#M20397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nasim,&lt;/P&gt;&lt;P&gt;Did you set STOPE bit in SOPT1? if not, executing STOP will cause a reset, then the debugger connection may lost. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 09:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286738#M20397</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-06-20T09:23:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286739#M20398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I have set the STOPE&amp;nbsp; bit and it is going in sleep mode and come out after RTC interrupt. I have managed to debug the unit with out the Debugger .But for future I need to find a way so that I waste less time in development.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 10:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286739#M20398</guid>
      <dc:creator>nasimimtiaz</dc:creator>
      <dc:date>2013-06-20T10:12:12Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286740#M20399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One Possibility is that my P&amp;amp;E USB Multilink is about four years old. May be it is not setting the ENBDM bit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2013 10:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286740#M20399</guid>
      <dc:creator>nasimimtiaz</dc:creator>
      <dc:date>2013-06-20T10:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286741#M20400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you share your project to me? then I can try it in my demo board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 06:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286741#M20400</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-06-21T06:03:10Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286742#M20401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The project is a GSM/GPRS&amp;nbsp; Tracking device It wont run without the hardware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 10:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286742#M20401</guid>
      <dc:creator>nasimimtiaz</dc:creator>
      <dc:date>2013-06-21T10:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286743#M20402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nasimimtiaz, how about your issue? did you try to use a new multilink?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2013 08:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286743#M20402</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-06-27T08:43:15Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286744#M20403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having the same problem. We are using a MCF51QE128 microcontroller and P&amp;amp;E Micro USB Multilink Interface.&lt;/P&gt;&lt;P&gt;Once my program enters stop mode and I activate another window (other than the debugger), the debugger loses the connection with the target. When I do not change focus of the window, I can halt the program and the connection works just fine and I can step into the next instruction. We are also using a multilink that is already a few years old.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas how to fix this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 09:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286744#M20403</guid>
      <dc:creator>Marcel</dc:creator>
      <dc:date>2013-07-02T09:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286745#M20404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marcel, I didn't try to click other windows before. let me raise such issue to P&amp;amp;E support team. Any response I get, I will update result here.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 09:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286745#M20404</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-07-02T09:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286746#M20405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marcel, As P&amp;amp;E's request, could you provide below information for th issue?&lt;/P&gt;&lt;P&gt;1 CodeWarrior version.&lt;/P&gt;&lt;P&gt;2. The version of firmware installed in their USB Multilink&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;3. your project with the code that causes the issues.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Thanks inadvance.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2013 05:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286746#M20405</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-07-04T05:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286747#M20406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just an update to let you know i am trying to strip the project, because we don't want to hand over the entire project with source code and everything. But with the stripped version so far, it seems the problem does not occur :-|&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CodeWarrior version we use is CodeWarrior for Microcontrollers, Classic Edition v6.3.1.&lt;/P&gt;&lt;P&gt;I don't know how to identify the firmware version. The dialog with the Connection Manager shows a blank field for firmware version. The port shows "USB-ML-12 Rev C (PE5516546)". Oh wait! The command window in the debugger shows "USB-ML-12 detected - Flash Version 5.81" .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2013 15:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286747#M20406</guid>
      <dc:creator>Marcel</dc:creator>
      <dc:date>2013-07-04T15:33:42Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286748#M20407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;:smileyplain:If so, it will be hard for us to find the reason.&amp;nbsp; Is it possible that the issue is caused by your software?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2013 08:34:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286748#M20407</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-07-05T08:34:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286749#M20408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think the problem is caused (mainly) by our software. The problem should be elsewhere, because there is nothing &lt;SPAN style="text-decoration: underline;"&gt;we&lt;/SPAN&gt; can do about it. The &lt;SPAN style="text-decoration: underline;"&gt;debugger&lt;/SPAN&gt; loses the connection!&lt;/P&gt;&lt;P&gt;I will try to see if I can work on this item again today, to make it reproduce again. But I'll first have to do some other things.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2013 08:40:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286749#M20408</guid>
      <dc:creator>Marcel</dc:creator>
      <dc:date>2013-07-05T08:40:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286750#M20409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok, no problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2013 08:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286750#M20409</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-07-05T08:58:54Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM in Stop  mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286751#M20410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was thinking, maybe the problem could be caused by the USB hub, which I have connected between the PC and the Multilink. Although the hub is a certified USB hub from D-Link and theoretically should not cause problems. I just ran some tests to find out if not using the hub would solve the problem, but unfortunately (or fortunately?) I cannot reproduce the problem anymore, even with our full project. That said, I think the problem should not be in our software, because the debugger lost its connection the last time (see previous post).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I won't have the opportunity to investigate the problem in the future if it comes back, but maybe this post might help others with the same problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2013 08:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-in-Stop-mode/m-p/286751#M20410</guid>
      <dc:creator>Marcel</dc:creator>
      <dc:date>2013-08-07T08:56:10Z</dc:date>
    </item>
  </channel>
</rss>