<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックExternal inputs to a microprocessor</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/External-inputs-to-a-microprocessor/m-p/284124#M20324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a 9S08AC32 in my design.&amp;nbsp; The board that I'm designing has connectors that external modules can plug-in.&amp;nbsp; When the modules is inserted, it pulls an I/O pin of the micro (pull-ups enabled) low.&amp;nbsp; My logic detects if the I/O pin is low then a module is plugged in.&amp;nbsp; I have 16 of these input pins.&amp;nbsp; Normally I would route these pins to a parallel load serial shift register and clock the results in.&amp;nbsp; Hopefully the module would only be inserted in when the power is off.&amp;nbsp; The connector is pinned so the module can only be plugged in one way.&amp;nbsp; I have 16 spared I/O pins.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any thoughts and/or opinions on this on going directly to the I/O's.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Barry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Oct 2013 20:38:35 GMT</pubDate>
    <dc:creator>barrygordon</dc:creator>
    <dc:date>2013-10-16T20:38:35Z</dc:date>
    <item>
      <title>External inputs to a microprocessor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/External-inputs-to-a-microprocessor/m-p/284124#M20324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a 9S08AC32 in my design.&amp;nbsp; The board that I'm designing has connectors that external modules can plug-in.&amp;nbsp; When the modules is inserted, it pulls an I/O pin of the micro (pull-ups enabled) low.&amp;nbsp; My logic detects if the I/O pin is low then a module is plugged in.&amp;nbsp; I have 16 of these input pins.&amp;nbsp; Normally I would route these pins to a parallel load serial shift register and clock the results in.&amp;nbsp; Hopefully the module would only be inserted in when the power is off.&amp;nbsp; The connector is pinned so the module can only be plugged in one way.&amp;nbsp; I have 16 spared I/O pins.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any thoughts and/or opinions on this on going directly to the I/O's.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Barry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2013 20:38:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/External-inputs-to-a-microprocessor/m-p/284124#M20324</guid>
      <dc:creator>barrygordon</dc:creator>
      <dc:date>2013-10-16T20:38:35Z</dc:date>
    </item>
    <item>
      <title>Re: External inputs to a microprocessor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/External-inputs-to-a-microprocessor/m-p/284125#M20325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Barry,&lt;/P&gt;&lt;P&gt;There is no issues with connecting right to the microcontroller from the outside world, meaning the connector.  The only thing that you will want to do is insert a 100 ohm resistor in series with all the spare i/o pins to limit any inrush current.  Possibly add a 0.1uF cap to each line as well for filtering.  We have many customers doing this in their designs as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2013 22:38:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/External-inputs-to-a-microprocessor/m-p/284125#M20325</guid>
      <dc:creator>michaelsteffenf</dc:creator>
      <dc:date>2013-10-16T22:38:47Z</dc:date>
    </item>
  </channel>
</rss>