<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PGA- Programmable Gain Amplifier in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PGA-Programmable-Gain-Amplifier/m-p/271934#M20173</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Florijan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The gain available from the PGA would seem to be unsufficient - the output from the PGA will increase the analog level to about 1.7 percent of full scale.&amp;nbsp; This would produce a maximum count of 71, giving an effective ADC resolution of about 6 bits.&amp;nbsp; The inclusion of an external low noise preamplifier, with a gain of 50, would improve the results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The effectiveness of your averaging process will be influenced by the number and timing of the individual readings.&amp;nbsp; If some of the fluctuation is due to the presence 50 Hz mains hum components, the readings should be taken over a 20 millisecond period, or a multiple, to average out the hum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jul 2013 02:21:03 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2013-07-16T02:21:03Z</dc:date>
    <item>
      <title>PGA- Programmable Gain Amplifier</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PGA-Programmable-Gain-Amplifier/m-p/271933#M20172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an application in which I need to sense voltage from 0-1.8 mV from pressure sensor. I am using PGA (32x) and 12bit ADC inside MC9S08MP mcu. So far everything works ok except ADC measurements are not&amp;nbsp; so stable. I am using software averaging to get more stable results. My question here is simple:&lt;/P&gt;&lt;P&gt;How to initialize ADC and PGA to get the best possible accuracy and stable results? Are there any tricks with this peripherals? The mcu bus frequency is 1MHz max.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Florijan &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2013 11:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PGA-Programmable-Gain-Amplifier/m-p/271933#M20172</guid>
      <dc:creator>Florijan</dc:creator>
      <dc:date>2013-07-15T11:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: PGA- Programmable Gain Amplifier</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PGA-Programmable-Gain-Amplifier/m-p/271934#M20173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Florijan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The gain available from the PGA would seem to be unsufficient - the output from the PGA will increase the analog level to about 1.7 percent of full scale.&amp;nbsp; This would produce a maximum count of 71, giving an effective ADC resolution of about 6 bits.&amp;nbsp; The inclusion of an external low noise preamplifier, with a gain of 50, would improve the results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The effectiveness of your averaging process will be influenced by the number and timing of the individual readings.&amp;nbsp; If some of the fluctuation is due to the presence 50 Hz mains hum components, the readings should be taken over a 20 millisecond period, or a multiple, to average out the hum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2013 02:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PGA-Programmable-Gain-Amplifier/m-p/271934#M20173</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2013-07-16T02:21:03Z</dc:date>
    </item>
  </channel>
</rss>