<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Sir, when i connect programmer with controller PCB for Programming then there is a message displays that MCU is not responding then what can i do? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Sir-when-i-connect-programmer-with-controller-PCB-for/m-p/270044#M20154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As the hint please check if the power of the MCU is ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;xwp &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Oct 2013 09:39:01 GMT</pubDate>
    <dc:creator>weapon</dc:creator>
    <dc:date>2013-10-10T09:39:01Z</dc:date>
    <item>
      <title>Sir, when i connect programmer with controller PCB for Programming then there is a message displays that MCU is not responding then what can i do?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Sir-when-i-connect-programmer-with-controller-PCB-for/m-p/270043#M20153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119669i79C9460DF942FC9F/image-size/large?v=v2&amp;amp;px=999" title="6692_6692.jpg" alt="6692_6692.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40956i77E6E93890DF0413/image-size/large?v=v2&amp;amp;px=999" title="prog fault.jpg" alt="prog fault.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2013 04:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Sir-when-i-connect-programmer-with-controller-PCB-for/m-p/270043#M20153</guid>
      <dc:creator>abhayshankar</dc:creator>
      <dc:date>2013-10-09T04:17:23Z</dc:date>
    </item>
    <item>
      <title>Re: Sir, when i connect programmer with controller PCB for Programming then there is a message displays that MCU is not responding then what can i do?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Sir-when-i-connect-programmer-with-controller-PCB-for/m-p/270044#M20154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As the hint please check if the power of the MCU is ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;xwp &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2013 09:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Sir-when-i-connect-programmer-with-controller-PCB-for/m-p/270044#M20154</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-10-10T09:39:01Z</dc:date>
    </item>
  </channel>
</rss>