<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 PWM on FTM2</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-on-FTM2/m-p/269098#M20130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm using MC9S08PT60 controller to generate a PWM using FTM2, using processor expert.I could generate the same on FTM0 and FTM1 and also could vary the duty cycle. But i want it on FTM2 so that I can control the speed of a DC motor, owing to the advantage that FTM2 supports complementary channels.Can anybody help on this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Aug 2013 10:32:21 GMT</pubDate>
    <dc:creator>pramodtm-b46240</dc:creator>
    <dc:date>2013-08-22T10:32:21Z</dc:date>
    <item>
      <title>PWM on FTM2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-on-FTM2/m-p/269098#M20130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm using MC9S08PT60 controller to generate a PWM using FTM2, using processor expert.I could generate the same on FTM0 and FTM1 and also could vary the duty cycle. But i want it on FTM2 so that I can control the speed of a DC motor, owing to the advantage that FTM2 supports complementary channels.Can anybody help on this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2013 10:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-on-FTM2/m-p/269098#M20130</guid>
      <dc:creator>pramodtm-b46240</dc:creator>
      <dc:date>2013-08-22T10:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: PWM on FTM2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-on-FTM2/m-p/269099#M20131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;We have a bldc motor demo in TWR-S08PT, whihc uses FTM2 to generate 6 pwm signal to control a bldc motors. you can take it as reference.&lt;/P&gt;&lt;P&gt;The demo is in attachment.&amp;nbsp; Hope it can be helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2013 08:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-on-FTM2/m-p/269099#M20131</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2013-08-23T08:04:38Z</dc:date>
    </item>
    <item>
      <title>Re: PWM on FTM2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-on-FTM2/m-p/269100#M20132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank u very much...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2013 05:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-on-FTM2/m-p/269100#M20132</guid>
      <dc:creator>pramodtm-b46240</dc:creator>
      <dc:date>2013-08-26T05:25:38Z</dc:date>
    </item>
  </channel>
</rss>