<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: HCS08 already programmed and temperature range</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-already-programmed-and-temperature-range/m-p/267112#M20077</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frantic Carlitos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were these answers helpful? Please keep us posted! :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Monica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Jun 2013 00:09:42 GMT</pubDate>
    <dc:creator>Monica</dc:creator>
    <dc:date>2013-06-13T00:09:42Z</dc:date>
    <item>
      <title>HCS08 already programmed and temperature range</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-already-programmed-and-temperature-range/m-p/267110#M20075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First question&lt;/P&gt;&lt;P&gt;S08JM60 microcontrollers are orderable already programmed (with firmware that let me to use it for jtag programming of another kinetics mcu)? Is there any parameter key in buy code that let me know this thing?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Second question&lt;/P&gt;&lt;P&gt;Is there any mcu of this family that has -40°:+105° temperature range?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2013 09:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-already-programmed-and-temperature-range/m-p/267110#M20075</guid>
      <dc:creator>franticcarlitos</dc:creator>
      <dc:date>2013-05-31T09:21:51Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 already programmed and temperature range</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-already-programmed-and-temperature-range/m-p/267111#M20076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frantic,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you buy the microcontroller, it will be blank. Maybe you want to build your own USBDM ? In this case have a look to S08JS16 versions which can be flashed throw the USB connection. It is also possible to buy USBDM on eBay for example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To answer you second question, no. S08JM devices are only available from -40°C to 85°C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joel Guittet&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Jun 2013 07:53:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-already-programmed-and-temperature-range/m-p/267111#M20076</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2013-06-02T07:53:47Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 already programmed and temperature range</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-already-programmed-and-temperature-range/m-p/267112#M20077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Frantic Carlitos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were these answers helpful? Please keep us posted! :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Monica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2013 00:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-already-programmed-and-temperature-range/m-p/267112#M20077</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-06-13T00:09:42Z</dc:date>
    </item>
  </channel>
</rss>