<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Weird Problem with current consumption with PA4 in STOP3 Mode in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Weird-Problem-with-current-consumption-with-PA4-in-STOP3-Mode/m-p/262505#M20032</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm developing a battery powered application using a PA4 device, the STOP3 mode, as it says in the datasheet, consumes about 1.4µA at 3v, And using an HP34401A I get almost exactly that 1.4µA, the problem is that when I put my finger near the PCB tracks the current consumption increases, it varies but it can jump up to 50µA, If I remove my finger it returns to 1.4µA does anybody has a clue about what's happening? How can it be possible that some noise or interference make it consume more current?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jan 2014 14:25:57 GMT</pubDate>
    <dc:creator>carloscuev</dc:creator>
    <dc:date>2014-01-28T14:25:57Z</dc:date>
    <item>
      <title>Weird Problem with current consumption with PA4 in STOP3 Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Weird-Problem-with-current-consumption-with-PA4-in-STOP3-Mode/m-p/262505#M20032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm developing a battery powered application using a PA4 device, the STOP3 mode, as it says in the datasheet, consumes about 1.4µA at 3v, And using an HP34401A I get almost exactly that 1.4µA, the problem is that when I put my finger near the PCB tracks the current consumption increases, it varies but it can jump up to 50µA, If I remove my finger it returns to 1.4µA does anybody has a clue about what's happening? How can it be possible that some noise or interference make it consume more current?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 14:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Weird-Problem-with-current-consumption-with-PA4-in-STOP3-Mode/m-p/262505#M20032</guid>
      <dc:creator>carloscuev</dc:creator>
      <dc:date>2014-01-28T14:25:57Z</dc:date>
    </item>
    <item>
      <title>Re: Weird Problem with current consumption with PA4 in STOP3 Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Weird-Problem-with-current-consumption-with-PA4-in-STOP3-Mode/m-p/262506#M20033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would estimate this is result of floating input(s). Add pullups or configure them to outputs (depending on what is connected to the pins)&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2014 15:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Weird-Problem-with-current-consumption-with-PA4-in-STOP3-Mode/m-p/262506#M20033</guid>
      <dc:creator>pavel_sadek</dc:creator>
      <dc:date>2014-01-28T15:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: Weird Problem with current consumption with PA4 in STOP3 Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Weird-Problem-with-current-consumption-with-PA4-in-STOP3-Mode/m-p/262507#M20034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That was it, just made all pins 0 before going to stop3 and voila! 1.4µA no matter what. Thank you very much, I've learned something new :smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2014 03:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Weird-Problem-with-current-consumption-with-PA4-in-STOP3-Mode/m-p/262507#M20034</guid>
      <dc:creator>carloscuev</dc:creator>
      <dc:date>2014-01-30T03:41:10Z</dc:date>
    </item>
  </channel>
</rss>