<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: ICG With External Oscilattor</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260780#M19985</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using a 4MHz external oscillator, the combination N = 10, R = 1 should correctly generate a 40 MHz DCO frequency, and a 20 MHz bus frequency.&amp;nbsp; This is on the upper DCO frequency limit.&amp;nbsp; It might pay to initially leave R at the default value of 2 whilst setting up FEE mode.&amp;nbsp; After lock has occurred, you would then set R = 1 as a separate process.&amp;nbsp; This will avoid the possibility of overclocking the MCU prior to lock occurring.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a bus frequency of 16 MHz, the only combination that will work is N = 8, R = 1.&amp;nbsp; If you attempt to set N = 16, this will exceed the maximum DCO frequency limit, and lock will not occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since you are using an external oscillator, rather than a crystal, it is unnecessary to set bit-5 of ICGC1.&amp;nbsp; This will free up the XTAL pin for GPIO use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2013 13:01:04 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2013-05-28T13:01:04Z</dc:date>
    <item>
      <title>ICG With External Oscilattor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260779#M19984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using an 9S08AC128 with an external 4.000MHz canned oscillator, and require a bus clock of 16.000MHz.&amp;nbsp; I've assumed I will need to switch to FEE mode, with N=16 and R=2.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To test my overall project I have a 32.000MHz oscillator attached, creating a 16.000MHz bus clock.&lt;/P&gt;&lt;P&gt;ICG_Init&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mov #%01010000,rICGC1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mov #%00000000,rICGC2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rts&lt;/P&gt;&lt;P&gt;The above code works fine.&amp;nbsp; I have a timer generating a 1Hz signal that flashes a LED and it's quite accurate as you would expect. Now it's time to swap over to the 4.000MHz oscillator.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Page 201 of the Reference Manual provides an example that generates a bus clock of 20 MHz from a 4MHz crystal. The code example is:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;ICG_Init&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;mov #%01111000,rICGC1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mov #%00110000,rICGC2 ;N=10, R=1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rts&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I run this code I get a bus clock substantially below 20 MHz (visible by a very slow flashing LED). My plan was to then change ICGC2 to N=16 and R=2 to generate my 16.000MHz bus clock.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Curiously page 202 of the same Reference Manual gives a different value for ICGC1 than the previous page for the same example, and I suspect that's a typo.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;Any suggestions about what I have overlooked?&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 10:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260779#M19984</guid>
      <dc:creator>davidboyd</dc:creator>
      <dc:date>2013-05-28T10:42:12Z</dc:date>
    </item>
    <item>
      <title>Re: ICG With External Oscilattor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260780#M19985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using a 4MHz external oscillator, the combination N = 10, R = 1 should correctly generate a 40 MHz DCO frequency, and a 20 MHz bus frequency.&amp;nbsp; This is on the upper DCO frequency limit.&amp;nbsp; It might pay to initially leave R at the default value of 2 whilst setting up FEE mode.&amp;nbsp; After lock has occurred, you would then set R = 1 as a separate process.&amp;nbsp; This will avoid the possibility of overclocking the MCU prior to lock occurring.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a bus frequency of 16 MHz, the only combination that will work is N = 8, R = 1.&amp;nbsp; If you attempt to set N = 16, this will exceed the maximum DCO frequency limit, and lock will not occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since you are using an external oscillator, rather than a crystal, it is unnecessary to set bit-5 of ICGC1.&amp;nbsp; This will free up the XTAL pin for GPIO use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 13:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260780#M19985</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2013-05-28T13:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: ICG With External Oscilattor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260781#M19986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply Mac.&lt;/P&gt;&lt;P&gt;Therefore are you suggesting the following for a 4MHz external oscillator generating a bus clock of 16MHz:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ICG_Init&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mov #%01011000,rICGC1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;RANGE=hi, CLKS=11(FLL engaged, external)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mov #%00100001,rICGC2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;N=8, R=2&lt;/P&gt;&lt;P&gt;icg_wait_lock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; brclr 3,rICGS1,icg_wait_lock&amp;nbsp;&amp;nbsp; ;wait for the FLL to lock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; mov #%00100000,rICGC2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;N=8, R=1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rts&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 13:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260781#M19986</guid>
      <dc:creator>davidboyd</dc:creator>
      <dc:date>2013-05-28T13:16:16Z</dc:date>
    </item>
    <item>
      <title>Re: ICG With External Oscilattor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260782#M19987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, this is what I had suggested.&amp;nbsp; Does it work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 16:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260782#M19987</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2013-05-28T16:09:44Z</dc:date>
    </item>
    <item>
      <title>Re: ICG With External Oscilattor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260783#M19988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mac,&lt;/P&gt;&lt;P&gt;Yes, that worked perfectly.&amp;nbsp; The wait for lock was essential.&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2013 13:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-With-External-Oscilattor/m-p/260783#M19988</guid>
      <dc:creator>davidboyd</dc:creator>
      <dc:date>2013-05-29T13:12:51Z</dc:date>
    </item>
  </channel>
</rss>