<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 9S08AC60 external ceramic resonator not locking in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259435#M19958</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have built two boards both with a 4Mhz Ceramic Resonator.&amp;nbsp; Both board, using the Cyclone Pro can be programmed and single step.&lt;/P&gt;&lt;P&gt;On one board the ceramic resonator is not locking (using a scope - no oscillator on either pin).&amp;nbsp; The code is set up as in example 2 of the manual.&amp;nbsp; The code is stuck on the while loop.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The ceramic resonator has the bypass capacitors and resistors embedded in the body.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ICGC1 = 0x30;&lt;/P&gt;&lt;P&gt;ICGC2 = 0x30;&lt;/P&gt;&lt;P&gt;/* Wait for LOCK bit */&lt;/P&gt;&lt;P&gt;while (!ICGS1_LOCK);&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The circuit ohms out Ok.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Any trouble hints on what to do next.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Apr 2013 22:06:04 GMT</pubDate>
    <dc:creator>barrygordon</dc:creator>
    <dc:date>2013-04-09T22:06:04Z</dc:date>
    <item>
      <title>9S08AC60 external ceramic resonator not locking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259435#M19958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have built two boards both with a 4Mhz Ceramic Resonator.&amp;nbsp; Both board, using the Cyclone Pro can be programmed and single step.&lt;/P&gt;&lt;P&gt;On one board the ceramic resonator is not locking (using a scope - no oscillator on either pin).&amp;nbsp; The code is set up as in example 2 of the manual.&amp;nbsp; The code is stuck on the while loop.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The ceramic resonator has the bypass capacitors and resistors embedded in the body.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ICGC1 = 0x30;&lt;/P&gt;&lt;P&gt;ICGC2 = 0x30;&lt;/P&gt;&lt;P&gt;/* Wait for LOCK bit */&lt;/P&gt;&lt;P&gt;while (!ICGS1_LOCK);&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The circuit ohms out Ok.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Any trouble hints on what to do next.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 22:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259435#M19958</guid>
      <dc:creator>barrygordon</dc:creator>
      <dc:date>2013-04-09T22:06:04Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08AC60 external ceramic resonator not locking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259436#M19959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mistyped when I enter the code:&lt;/P&gt;&lt;P&gt;ICGC1 = 0x78;&lt;/P&gt;&lt;P&gt;ICGC2 = 0x30;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 00:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259436#M19959</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-04-11T00:23:22Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08AC60 external ceramic resonator not locking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259437#M19960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To confirm that the ceramic resonator actually contains embedded resistance, the quiescent voltage measured at each of the pins should be approximately equal at one half Vdd.&amp;nbsp; The oscilloscope probe setting will need to be x10 for 10M ohm input resistance.&amp;nbsp; If the two voltages significantly differ from each other, with voltages close to either supply rail, the particular resonator may not contain sufficiently low embedded resistance.&amp;nbsp; I would expect a value of about 1M ohm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the capacitance ot the oscilloscope probe is too high, it is possible for the measurement process to cause oscillations to cease.&amp;nbsp; Check for oscillation at both pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 01:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259437#M19960</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2013-04-11T01:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08AC60 external ceramic resonator not locking</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259438#M19961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The voltage was the same on each side approx 1/2 Vdd.&amp;nbsp; My scope probes are x10.&lt;/P&gt;&lt;P&gt;I changed out the resonator with a spare and that fixed the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after rechecking the resonator again, it appeared that there was no embedded resistor - I added a 1 meg ohm resistor - that fixed the problem - built 7 modules and all work. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2013 01:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-external-ceramic-resonator-not-locking/m-p/259438#M19961</guid>
      <dc:creator>barrygordon</dc:creator>
      <dc:date>2013-04-12T01:10:46Z</dc:date>
    </item>
  </channel>
</rss>