<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC9S08JM60 USB-CDC device problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM60-USB-CDC-device-problem/m-p/257645#M19912</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try by modifying the inf file to add one more line as below&lt;/P&gt;&lt;P&gt;XXXXXXXXX (the string that you use in the inf file), USB\VID_2504&amp;amp;PID_0300&amp;amp;MI_00&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Apr 2013 01:37:09 GMT</pubDate>
    <dc:creator>DerekLau</dc:creator>
    <dc:date>2013-04-11T01:37:09Z</dc:date>
    <item>
      <title>MC9S08JM60 USB-CDC device problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM60-USB-CDC-device-problem/m-p/257644#M19911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used the last USB-STACK proposed by freescale (the 4.0.3) with a MC9S08JM60 to develop a USB-CDC application.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With my DEMOJM development card, I have used the example provided in the Stack ("C: \ Freescale \ Freescale USB Stack v4.0.3 \ Source \ Device \ app \ cdc \ CW10 \ s08usbjm60"). I also used tools from the excelent blog "mcuoneclipse.com" (&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fmcuoneclipse.com%2F2012%2F03%2F10%2Fusb-or-not-cdc-with-processor-expert%2F" rel="nofollow" target="_blank"&gt;USB or not: CDC with Processor Expert | MCU on Eclipse&lt;/A&gt;). I have obtained two USB-CDC devices. Well !&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I connect my USB-CDC devices directly into an USB port on my PC, there is no problem, the devices are both detected and the driver (CDC.inf) works. I can connect and communicate with my JM60 demo board across the CDC protocol.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My problem is when I connect the USB-CDC devices to my USB over IP module (StarTech - Part # USB1000IP). The USB devices are detected and appear inside the Windows Device Manager, but not installed inside the ports (COM and LTP) section. And the device is not available for communication. I tried two other USB over IP modules from other manufacturers, and I have the same problems. Worse, if I try to force the driver installation, Windows 7-64 or XP-32 show me the blue screen.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For info : inside the Windows Device Manager, the device instance id is : "USB\VID_2504&amp;amp;PID_0300&amp;amp;REV_0002" when I connect the device directly to USB.&lt;/P&gt;&lt;P&gt;It becomes "USB\Vid_2504&amp;amp;Pid_0300&amp;amp;Rev_0002&amp;amp;MI_00" when I use the&amp;nbsp; USB over IP module&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;Do you have a solution? An idea? A line of thought&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance for your help.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Stéphane&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Courier New'; color: black;"&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Courier New'; color: black;"&gt; &lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 07:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM60-USB-CDC-device-problem/m-p/257644#M19911</guid>
      <dc:creator>stéphanec</dc:creator>
      <dc:date>2013-04-09T07:02:42Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08JM60 USB-CDC device problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM60-USB-CDC-device-problem/m-p/257645#M19912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try by modifying the inf file to add one more line as below&lt;/P&gt;&lt;P&gt;XXXXXXXXX (the string that you use in the inf file), USB\VID_2504&amp;amp;PID_0300&amp;amp;MI_00&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 01:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM60-USB-CDC-device-problem/m-p/257645#M19912</guid>
      <dc:creator>DerekLau</dc:creator>
      <dc:date>2013-04-11T01:37:09Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08JM60 USB-CDC device problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM60-USB-CDC-device-problem/m-p/257646#M19913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've thought about this solution. Unfortunately it does not work (crash the PC at driver installation).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stéphane&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2013 06:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM60-USB-CDC-device-problem/m-p/257646#M19913</guid>
      <dc:creator>stéphanec</dc:creator>
      <dc:date>2013-04-11T06:50:08Z</dc:date>
    </item>
  </channel>
</rss>