<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with CW10.5 debugger and PA4 VTG cpu with flash security option ON in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-CW10-5-debugger-and-PA4-VTG-cpu-with-flash-security/m-p/252649#M19849</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Even a simple led blinking project seems to show the problem. If I set the NV_FSEC_INIT @0x0000FF7FU = 0x7DU the application would not start after bdm removing and issueing a cpu reset. During flash programming a " device is secure. Erase to unsecure" message appear but then tha application would not start at all. It seems the flash is secured prior to dco trimming and flash updating......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Sep 2013 16:23:05 GMT</pubDate>
    <dc:creator>gpadam</dc:creator>
    <dc:date>2013-09-26T16:23:05Z</dc:date>
    <item>
      <title>Problem with CW10.5 debugger and PA4 VTG cpu with flash security option ON</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-CW10-5-debugger-and-PA4-VTG-cpu-with-flash-security/m-p/252649#M19849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Even a simple led blinking project seems to show the problem. If I set the NV_FSEC_INIT @0x0000FF7FU = 0x7DU the application would not start after bdm removing and issueing a cpu reset. During flash programming a " device is secure. Erase to unsecure" message appear but then tha application would not start at all. It seems the flash is secured prior to dco trimming and flash updating......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Sep 2013 16:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-CW10-5-debugger-and-PA4-VTG-cpu-with-flash-security/m-p/252649#M19849</guid>
      <dc:creator>gpadam</dc:creator>
      <dc:date>2013-09-26T16:23:05Z</dc:date>
    </item>
  </channel>
</rss>