<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックI2C Communication</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I2C-Communication/m-p/248542#M19775</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I'm working with 2u (MC9S08SH8CWJ and MC9S08QG4) the problem is that the slave doesn't respond anything, as the protocol indicate first I send a byte(with an specific add 0x84) and then read a byte saved in a void byte in master mode,&amp;nbsp; and in slave mode i'm just send a data with an pointer that point an specif address with content.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the I2C methods and function, but doesn't work, I see an Oscilloscope like the Master send the start conditional, slave address, and the&amp;nbsp; write bit, but like never receive the acknowledge, so i think that problem is slave rigth? have you any idea like repair? &lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337763"&gt;SL6TXRX.rar&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Dec 2013 16:07:07 GMT</pubDate>
    <dc:creator>alancalonico</dc:creator>
    <dc:date>2013-12-06T16:07:07Z</dc:date>
    <item>
      <title>I2C Communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I2C-Communication/m-p/248542#M19775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I'm working with 2u (MC9S08SH8CWJ and MC9S08QG4) the problem is that the slave doesn't respond anything, as the protocol indicate first I send a byte(with an specific add 0x84) and then read a byte saved in a void byte in master mode,&amp;nbsp; and in slave mode i'm just send a data with an pointer that point an specif address with content.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the I2C methods and function, but doesn't work, I see an Oscilloscope like the Master send the start conditional, slave address, and the&amp;nbsp; write bit, but like never receive the acknowledge, so i think that problem is slave rigth? have you any idea like repair? &lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337763"&gt;SL6TXRX.rar&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Dec 2013 16:07:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/I2C-Communication/m-p/248542#M19775</guid>
      <dc:creator>alancalonico</dc:creator>
      <dc:date>2013-12-06T16:07:07Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I2C-Communication/m-p/248543#M19776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check if the power supply/oscillator of slave is ok, and the chip is working;&lt;/P&gt;&lt;P&gt;then check I2C start condition requirements are met (rise time, fall time, high/low before/after timing requirements )&lt;/P&gt;&lt;P&gt;then check its slave address is correct, and same as you see on oscilloscope,&lt;/P&gt;&lt;P&gt;then check if slave chip is not in master mode, with its status/control register.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jan 2014 06:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/I2C-Communication/m-p/248543#M19776</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-01-02T06:33:56Z</dc:date>
    </item>
  </channel>
</rss>