<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JM60 Proyect design in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247471#M19724</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you have to program the JM60 of the USBDM first with a BDM tool before you can use it. Only the JS16 version has a bootloader in ROM. So at first you have to get a BDM tool or build the JS16 version. The USBDM code and schematics can be found at sourceforges USBDM site. After Programming you can test the chip via the BDM tool.&lt;/P&gt;&lt;P&gt;You will go best if you build or get a JS16 USBDM for programming and debugging and test the JM60 in the circuit where it is needed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Eckhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 May 2013 12:51:54 GMT</pubDate>
    <dc:creator>eckhard</dc:creator>
    <dc:date>2013-05-21T12:51:54Z</dc:date>
    <item>
      <title>JM60 Proyect design</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247470#M19723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;jmHi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Im new to work with the JM60, and i have to make a proyect with it. I have been reading and i would like like to know if i'm right about the next process:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. I have a MC9S08JM60CLD 44QFP&lt;/P&gt;&lt;P&gt;2. Then program the JM60 building a USBDM, like the one in the link:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fusbdm.sourceforge.net%2FUSBDM_V4.9%2FUSBDM_JMxx%2Fhtml%2Findex.html" rel="nofollow" target="_blank"&gt;http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JMxx/html/index.html&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;3. I need a special type of programming code using the USBDM?&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;4. When i have to programmed the JM60, how can i test if it works?, i have to desolder and place it (the JM60)&amp;nbsp; on a new&amp;nbsp; PCB for testing?&lt;/P&gt;&lt;P&gt;5. There is possible to made a cheap pcb to program and test?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2013 16:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247470#M19723</guid>
      <dc:creator>hommmer</dc:creator>
      <dc:date>2013-05-20T16:49:41Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 Proyect design</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247471#M19724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you have to program the JM60 of the USBDM first with a BDM tool before you can use it. Only the JS16 version has a bootloader in ROM. So at first you have to get a BDM tool or build the JS16 version. The USBDM code and schematics can be found at sourceforges USBDM site. After Programming you can test the chip via the BDM tool.&lt;/P&gt;&lt;P&gt;You will go best if you build or get a JS16 USBDM for programming and debugging and test the JM60 in the circuit where it is needed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Eckhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2013 12:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247471#M19724</guid>
      <dc:creator>eckhard</dc:creator>
      <dc:date>2013-05-21T12:51:54Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 Proyect design</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247472#M19725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Genner!&lt;/P&gt;&lt;P&gt;Was this suggestion helpful? Don't forget to keep us posted!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Monica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2013 19:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247472#M19725</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-05-28T19:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: JM60 Proyect design</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247473#M19726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks very usefull info&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2013 04:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JM60-Proyect-design/m-p/247473#M19726</guid>
      <dc:creator>hommmer</dc:creator>
      <dc:date>2013-05-29T04:25:06Z</dc:date>
    </item>
  </channel>
</rss>