<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S08 SCI Transmit Issue in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-Transmit-Issue/m-p/245392#M19678</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I did try the code. After changing the SCI2s to SCI0s I was unable to get it to work either. I noticed that there was a read of SCI0_S1 (which clears the flags) just before the while that waits for the flag to clear in the example that you linked. I put that in my code and it appears to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Aug 2013 20:24:00 GMT</pubDate>
    <dc:creator>gregoryberardi</dc:creator>
    <dc:date>2013-08-08T20:24:00Z</dc:date>
    <item>
      <title>S08 SCI Transmit Issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-Transmit-Issue/m-p/245390#M19676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The attached code is what I'm using to try to send data out the sci tx port. The problem I am having is that I'm not seeing anything on the output (PTA3).&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help is appreciated. Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337753"&gt;main.c.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2013 03:09:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-Transmit-Issue/m-p/245390#M19676</guid>
      <dc:creator>gregoryberardi</dc:creator>
      <dc:date>2013-08-08T03:09:49Z</dc:date>
    </item>
    <item>
      <title>Re: S08 SCI Transmit Issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-Transmit-Issue/m-p/245391#M19677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;can you please check this thread? i think it should help you: &lt;/SPAN&gt;&lt;A class="jive-link-message-small" data-containerid="2016" data-containertype="14" data-objectid="330916" data-objecttype="2" href="https://community.freescale.com/message/330916#330916"&gt;https://community.freescale.com/message/330916#330916&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2013 03:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-Transmit-Issue/m-p/245391#M19677</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2013-08-08T03:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: S08 SCI Transmit Issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-Transmit-Issue/m-p/245392#M19678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I did try the code. After changing the SCI2s to SCI0s I was unable to get it to work either. I noticed that there was a read of SCI0_S1 (which clears the flags) just before the while that waits for the flag to clear in the example that you linked. I put that in my code and it appears to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2013 20:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-Transmit-Issue/m-p/245392#M19678</guid>
      <dc:creator>gregoryberardi</dc:creator>
      <dc:date>2013-08-08T20:24:00Z</dc:date>
    </item>
  </channel>
</rss>