<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Example code for internal ADC of MC9S08DZ96</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Example-code-for-internal-ADC-of-MC9S08DZ96/m-p/245247#M19675</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;You can download the dz60_demo.zip from the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.axman.com/content/demo9s08dz60"&gt;http://www.axman.com/content/demo9s08dz60&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also you can check the samples that are install with CodeWarrior the normal folder is &lt;/P&gt;&lt;P&gt;C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\(CodeWarrior_Examples)\HCS08\Evaluation Board Examples\EVB9S08DZ60\C&lt;BR /&gt;These samples are for the Evaluation board but you can check the initialization and use it for the DEMO, I believe that the two board has the same package.&lt;BR /&gt;On this folder you can find a sample for CAN, LIN, SCI and the demo that use the ADC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jennie&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Apr 2013 02:18:39 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2013-04-29T02:18:39Z</dc:date>
    <item>
      <title>Example code for internal ADC of MC9S08DZ96</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Example-code-for-internal-ADC-of-MC9S08DZ96/m-p/245245#M19673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am evaluating MC9S08DZ96 for one of the application and interested in testing ADC performance before making decision on ADC and controller. I have evaluation kit with me, is there sample code for internal ADC of MC9S08DZ96, which can be used for basic evaluation testing purpose??&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;P&gt;Manoj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Mar 2013 05:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Example-code-for-internal-ADC-of-MC9S08DZ96/m-p/245245#M19673</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-03-29T05:54:38Z</dc:date>
    </item>
    <item>
      <title>Re: Example code for internal ADC of MC9S08DZ96</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Example-code-for-internal-ADC-of-MC9S08DZ96/m-p/245246#M19674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did you find anything useful?&lt;/P&gt;&lt;P&gt;i'm in the same situation...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2013 13:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Example-code-for-internal-ADC-of-MC9S08DZ96/m-p/245246#M19674</guid>
      <dc:creator>GMVS</dc:creator>
      <dc:date>2013-04-26T13:27:25Z</dc:date>
    </item>
    <item>
      <title>Re: Example code for internal ADC of MC9S08DZ96</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Example-code-for-internal-ADC-of-MC9S08DZ96/m-p/245247#M19675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;You can download the dz60_demo.zip from the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.axman.com/content/demo9s08dz60"&gt;http://www.axman.com/content/demo9s08dz60&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Also you can check the samples that are install with CodeWarrior the normal folder is &lt;/P&gt;&lt;P&gt;C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\(CodeWarrior_Examples)\HCS08\Evaluation Board Examples\EVB9S08DZ60\C&lt;BR /&gt;These samples are for the Evaluation board but you can check the initialization and use it for the DEMO, I believe that the two board has the same package.&lt;BR /&gt;On this folder you can find a sample for CAN, LIN, SCI and the demo that use the ADC. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jennie&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2013 02:18:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Example-code-for-internal-ADC-of-MC9S08DZ96/m-p/245247#M19675</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2013-04-29T02:18:39Z</dc:date>
    </item>
  </channel>
</rss>