<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 68HC711E9CFN2 Replacement in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243058#M19637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found it … 11ma in the Wait mode and 18ma in the active mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tnx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tuWolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Feb 2014 19:58:29 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2014-02-20T19:58:29Z</dc:date>
    <item>
      <title>68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243048#M19627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a design around the 68HC711E9FN2 and we want to migrate the software, if possible to a new processor.&amp;nbsp; Does anyone have some suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 19:32:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243048#M19627</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-02-18T19:32:35Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243049#M19628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would highly recommend you to consider a redesign, all HC11 devices are being discontinued and we are also in the process of removing support for such part families, there is no pin to pin replacement to your chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;here you have two mcu families perfectly capable of replacing your current device, the natural replacement would be an 8 bit device, however there's a highly code compatible 16-bit family , I list both of them below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S08AW: 8-bit Microcontrollers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Features&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5-volt operational voltage&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Electromagnetic compatibility&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; High-performance S08 8-bit core&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wide peripheral offerings&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; This product is included in Freescale’s product longevity program, with assured supply for a minimum of 15 years after launch&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Product Specifications&lt;/P&gt;&lt;P&gt;Internal Flash (kByte)&amp;nbsp;&amp;nbsp; 60, 48, 32, 16, 8&lt;/P&gt;&lt;P&gt;I/O Pins&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 34, 38, 54, 22, 35&lt;/P&gt;&lt;P&gt;Serial Interface - Type&amp;nbsp; SCI, SPI, I2C, SPI&lt;/P&gt;&lt;P&gt;Additional Features&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; COP, KBI, POR, Temperature Sensor, Low Voltage Detect, Real-Time Clock, LVI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Homepage:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S08AW&amp;amp;nodeId=01624684491437"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S08AW&amp;amp;nodeId=01624684491437&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S12A: Microcontroller&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Features&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16-bit HCS12 CPU&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Upward compatible with M68HC11 instruction set&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Interrupt stacking and programmer's model identical to M68HC11&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Instruction pipe&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Enhanced indexed addressing&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Multiplexed external bus&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Memory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 512 KB flash EEPROM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4 KB EEPROM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 14 KB RAM&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Two 8-channel ADCs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 10-bit resolution&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Software compatible modules&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Product Specifications&lt;/P&gt;&lt;P&gt;Internal Flash (kByte)&amp;nbsp;&amp;nbsp; 128, 512, 32, 64, 256&lt;/P&gt;&lt;P&gt;EEPROM (kByte)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2, 1, 4&lt;/P&gt;&lt;P&gt;Serial Interface - Type&amp;nbsp; SCI, SPI, I2C, SPI, SPI&lt;/P&gt;&lt;P&gt;I/O Pins&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 59, 91&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Homepage:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12A&amp;amp;nodeId=0162468636K100"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12A&amp;amp;nodeId=0162468636K100&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 02:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243049#M19628</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-02-19T02:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243050#M19629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the technical update.  I was reading some of the comments on the HCS12(X) as a better conversion for my software modules rather than going to the HCS08.  Is this true?   Would you mind explaining the difference between the two processors?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My application is a low current design.  Does the current consumption compare between the HC11 and the HCS08/12?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What development packages do I need to purchase to work with the new processor and what software compilers do I need?  Will the software work that I am using for the 68HC11 on the HCS08/12?  All my work has been in Assembler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry Urbanowski&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TU Wolf Rf Designs Inc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 04:17:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243050#M19629</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-02-19T04:17:19Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243051#M19630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If your old code is done in assembler, then I think you should prefer S12. You can recompile your old HC11 code and it would even work, if not:&lt;/P&gt;&lt;P&gt;- not 100.0% compatible peripherals. You may need to revise your old drivers&lt;/P&gt;&lt;P&gt;- different address maps&lt;/P&gt;&lt;P&gt;- faster execution time, software delays need to be revised&lt;/P&gt;&lt;P&gt;- 2 times faster bus clock from the same crystal clock&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S08 is upgrade for HC08. S12 is upgrade for HC11. If your old code was done in C, then I would suggest using S08, since it is still faster than HC11. &lt;/P&gt;&lt;P&gt;To narrow S12 overview, I assume you don't need a lot of pins and prefer smaller (less pins) packages? If so then I think you should consider S12P family. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 09:14:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243051#M19630</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2014-02-19T09:14:29Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243052#M19631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your insight into the S12 and the code.  I read some comments on line about this issue of porting the software over to the new processor.  If we can do it with less issues, it is best to use the S12.  All our code is in Assembler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you mind providing me with a list of Development tools we will have to get to proceed on this migration path?  How do we get a couple of samples of the S12?  &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tuWolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 16:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243052#M19631</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-02-19T16:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243053#M19632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you mind sending me some technical data on the S12P?  I think we still have some spare pins we are not using on the HC711, so no use having a pile of unused pins!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;P&gt;tuWolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 19:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243053#M19632</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-02-19T19:20:56Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243054#M19633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;all the s12p related information is in its web page: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12P&amp;amp;lang_cd=en&amp;amp;webpageId=M0zGQK100&amp;amp;nodeId=0162468636K100&amp;amp;fromPage=tax"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S12P&amp;amp;lang_cd=en&amp;amp;webpageId=M0zGQK100&amp;amp;nodeId=0162468636K100&amp;amp;fromPage=tax&lt;/A&gt;&lt;SPAN&gt; hope this helps!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 03:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243054#M19633</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-02-20T03:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243055#M19634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jennie.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tuWolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 03:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243055#M19634</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-02-20T03:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243056#M19635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are welcome! please feel free to mark&amp;nbsp; "Correct Answer" and "Helpful Answer". thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 05:08:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243056#M19635</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-02-20T05:08:13Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243057#M19636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you provide me with the current consumption of the MC9S12P64?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I couldn’t seem to find it in the s12 reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tuWolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 19:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243057#M19636</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-02-20T19:49:29Z</dc:date>
    </item>
    <item>
      <title>Re: 68HC711E9CFN2 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243058#M19637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found it … 11ma in the Wait mode and 18ma in the active mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tnx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Terry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tuWolf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 19:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/68HC711E9CFN2-Replacement/m-p/243058#M19637</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-02-20T19:58:29Z</dc:date>
    </item>
  </channel>
</rss>