<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: AN1857 RS232 optoisolation interface</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242149#M19601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the optoisolated interface to work correctly when sending data to the PC, the signal at pin 7 (RTS) need to be set active by the PC, to achieve a voltage level of about +12 volts.&amp;nbsp; At the same time, the signal at pin 4 (DTR) should remain inactive, to retain the negative voltage level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Mar 2013 02:57:22 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2013-03-27T02:57:22Z</dc:date>
    <item>
      <title>AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242147#M19599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;I built a Hardware connection for MC9S08MP16, which is the same as described in app note AN1857, page 13. I try to communicate using Freemaster, with correct Baud rate setting. &lt;SPAN style="font-style: inherit; font-size: 10pt; font-family: inherit;"&gt;Unfortunately, it doesn't work. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;When I use P&amp;amp;E micro debugger, the communication is fine.&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;I measured my PC and found both pin 4 and pin 7 is of voltage around -11V. Anyone has an idea about this configuration?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Thanks&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;Ed&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2013 17:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242147#M19599</guid>
      <dc:creator>edjiang</dc:creator>
      <dc:date>2013-03-26T17:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242148#M19600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need insert the serial driver files into the project if you’re going to communicate via serial connection.  They are available on the Freescale web site in the Freemaster page.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2013 18:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242148#M19600</guid>
      <dc:creator>michaelsteffenf</dc:creator>
      <dc:date>2013-03-26T18:15:52Z</dc:date>
    </item>
    <item>
      <title>Re: AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242149#M19601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the optoisolated interface to work correctly when sending data to the PC, the signal at pin 7 (RTS) need to be set active by the PC, to achieve a voltage level of about +12 volts.&amp;nbsp; At the same time, the signal at pin 4 (DTR) should remain inactive, to retain the negative voltage level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 02:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242149#M19601</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2013-03-27T02:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242150#M19602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. I didn't find the files on the webpage "FreeMASTER Run-Time Debugging Tool". Could you please send me the link to the files or a screenshot of the webpage? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 08:13:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242150#M19602</guid>
      <dc:creator>edjiang</dc:creator>
      <dc:date>2013-03-27T08:13:42Z</dc:date>
    </item>
    <item>
      <title>Re: AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242151#M19603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the explanation. Should I do anything about this voltage setting? or it is done automatically by Freemaster?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 08:15:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242151#M19603</guid>
      <dc:creator>edjiang</dc:creator>
      <dc:date>2013-03-27T08:15:24Z</dc:date>
    </item>
    <item>
      <title>Re: AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242152#M19604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;forgot to mention that I use the "real" serial com port, NOT USB port.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 14:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242152#M19604</guid>
      <dc:creator>edjiang</dc:creator>
      <dc:date>2013-03-27T14:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242153#M19605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you install the serial source code into your project?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 14:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242153#M19605</guid>
      <dc:creator>michaelsteffenf</dc:creator>
      <dc:date>2013-03-27T14:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: AN1857 RS232 optoisolation interface</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242154#M19606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;that is the point. I don't know anything about the serial source code and I didn't find any information from the Freemaster webpage. Previously, I use P&amp;amp;E micro debugger, it works fine with Freemaster, which means my project code is okay. Now I need to communicate only using com port, that is the problem I have now. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2013 17:24:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN1857-RS232-optoisolation-interface/m-p/242154#M19606</guid>
      <dc:creator>edjiang</dc:creator>
      <dc:date>2013-03-27T17:24:48Z</dc:date>
    </item>
  </channel>
</rss>