<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: need help: can CASM08Z.EXE generate .s19 for HCS08 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/need-help-can-CASM08Z-EXE-generate-s19-for-HCS08/m-p/129438#M1954</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Ty for reply, but I still can't make my AW mcu working &amp;gt;.&amp;lt;. Was wondering if casm08.exe was the cause.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Sep 2006 11:13:38 GMT</pubDate>
    <dc:creator>Sany</dc:creator>
    <dc:date>2006-09-07T11:13:38Z</dc:date>
    <item>
      <title>need help: can CASM08Z.EXE generate .s19 for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/need-help-can-CASM08Z-EXE-generate-s19-for-HCS08/m-p/129436#M1952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi all,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; I used CASM08Z.EXE generate .s19 HC08. But my question now, is it possible to use the same method for HCS08? Is the .s19 format same for both HC08 and HCS08?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; Ty in advance for answering my questions.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2006 08:59:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/need-help-can-CASM08Z-EXE-generate-s19-for-HCS08/m-p/129436#M1952</guid>
      <dc:creator>Sany</dc:creator>
      <dc:date>2006-09-07T08:59:16Z</dc:date>
    </item>
    <item>
      <title>Re: need help: can CASM08Z.EXE generate .s19 for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/need-help-can-CASM08Z-EXE-generate-s19-for-HCS08/m-p/129437#M1953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Sany,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;The CASM08Z assembler will handle all instructions common to both the HC08 and HCS08 devices.&amp;nbsp; However, it does not assemble instructions that are unique to the HCS08.&amp;nbsp; A CASM assembler to handle the HCS08 would need to be purchased from P&amp;amp;E - it is not a free download.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;The S19 format should be the same for both types of device.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2006 09:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/need-help-can-CASM08Z-EXE-generate-s19-for-HCS08/m-p/129437#M1953</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2006-09-07T09:57:11Z</dc:date>
    </item>
    <item>
      <title>Re: need help: can CASM08Z.EXE generate .s19 for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/need-help-can-CASM08Z-EXE-generate-s19-for-HCS08/m-p/129438#M1954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Ty for reply, but I still can't make my AW mcu working &amp;gt;.&amp;lt;. Was wondering if casm08.exe was the cause.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2006 11:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/need-help-can-CASM08Z-EXE-generate-s19-for-HCS08/m-p/129438#M1954</guid>
      <dc:creator>Sany</dc:creator>
      <dc:date>2006-09-07T11:13:38Z</dc:date>
    </item>
  </channel>
</rss>