<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i need your help in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/i-need-your-help/m-p/237786#M19522</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am in beginning part of code warrior programming. i want to write the c and assembly coding for M9S08SH8. so what are the procedures i need to take to write the program well. i want the many sample code for 8bit M9S08SH8. if u have any material means please give me. u can also send the link which is available this. please help me. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 26 Jan 2013 13:31:37 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2013-01-26T13:31:37Z</dc:date>
    <item>
      <title>i need your help</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/i-need-your-help/m-p/237786#M19522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am in beginning part of code warrior programming. i want to write the c and assembly coding for M9S08SH8. so what are the procedures i need to take to write the program well. i want the many sample code for 8bit M9S08SH8. if u have any material means please give me. u can also send the link which is available this. please help me. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Jan 2013 13:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/i-need-your-help/m-p/237786#M19522</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-01-26T13:31:37Z</dc:date>
    </item>
    <item>
      <title>Re: i need your help</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/i-need-your-help/m-p/237787#M19523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sabha,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I highly recommend starting your project using Processor Expert.&amp;nbsp; This will create a project template into which you should be able to easily write your own code.&amp;nbsp; Processor Expert can also be used to create initialization and interface software for the MCU's peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the risk of patting my own back, I suggest also taking a look at a couple of my own blog entries:&lt;/P&gt;&lt;P&gt;The Bare Metal Enthusiast:&lt;/P&gt;&lt;P&gt;Start at the Beginning:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/community/the-embedded-beat/blog/2012/02/08/the-bare-metal-enthusiast-start-at-the-beginning"&gt;https://community.freescale.com/community/the-embedded-beat/blog/2012/02/08/the-bare-metal-enthusiast-start-at-the-beginning&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can C clearly:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/community/the-embedded-beat/blog/2012/03/06/the-bare-metal-enthusiast-i-can-c-clearly"&gt;https://community.freescale.com/community/the-embedded-beat/blog/2012/03/06/the-bare-metal-enthusiast-i-can-c-clearly&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Derrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2013 20:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/i-need-your-help/m-p/237787#M19523</guid>
      <dc:creator>Derrick</dc:creator>
      <dc:date>2013-01-29T20:09:38Z</dc:date>
    </item>
  </channel>
</rss>