<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: doubts the BDM in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/doubts-the-BDM/m-p/235935#M19490</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isaac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As all MC9S08xxx MC9S08SE8yyy may be programmed with an universal USB Multilink programmer from PEmicro or by a cheaper OSBDM programmer which has some disadvantages when running from CodeWarrior 6.3 (it cannot trim internal oscillator by default).&lt;/P&gt;&lt;P&gt;Another possibility is to use the buried USBMultilink programmer in the DEMO9S08SE8 evaluation board to program external in-circuit uCU of the same series (the program, while is a complete PEmicro multilink is software bounded to program only -SE series).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S08 and HCS08 are synonymous but the latter is no more used. Do not confuse with HC08 from the older 68HC908xx series which are pretty different in CPU specifications and lower in performance. They uses also different, much complicate, in-circuit programming and tools.&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Jan 2013 00:02:38 GMT</pubDate>
    <dc:creator>Encoder1</dc:creator>
    <dc:date>2013-01-25T00:02:38Z</dc:date>
    <item>
      <title>doubts the BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/doubts-the-BDM/m-p/235933#M19488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;if a BDM, HCS08 series program.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;can program the "MC9S08SE8CRL"?,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;or is there except for a micros?,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;I'm new to microcontrollers&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 18:55:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/doubts-the-BDM/m-p/235933#M19488</guid>
      <dc:creator>isaacmartinezsa</dc:creator>
      <dc:date>2013-01-24T18:55:09Z</dc:date>
    </item>
    <item>
      <title>Re: doubts the BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/doubts-the-BDM/m-p/235934#M19489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Same thing that S08 HCS08,&lt;/P&gt;&lt;P&gt;if yes why they put HC?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 19:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/doubts-the-BDM/m-p/235934#M19489</guid>
      <dc:creator>isaacmartinezsa</dc:creator>
      <dc:date>2013-01-24T19:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: doubts the BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/doubts-the-BDM/m-p/235935#M19490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isaac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As all MC9S08xxx MC9S08SE8yyy may be programmed with an universal USB Multilink programmer from PEmicro or by a cheaper OSBDM programmer which has some disadvantages when running from CodeWarrior 6.3 (it cannot trim internal oscillator by default).&lt;/P&gt;&lt;P&gt;Another possibility is to use the buried USBMultilink programmer in the DEMO9S08SE8 evaluation board to program external in-circuit uCU of the same series (the program, while is a complete PEmicro multilink is software bounded to program only -SE series).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S08 and HCS08 are synonymous but the latter is no more used. Do not confuse with HC08 from the older 68HC908xx series which are pretty different in CPU specifications and lower in performance. They uses also different, much complicate, in-circuit programming and tools.&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 00:02:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/doubts-the-BDM/m-p/235935#M19490</guid>
      <dc:creator>Encoder1</dc:creator>
      <dc:date>2013-01-25T00:02:38Z</dc:date>
    </item>
  </channel>
</rss>