<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 MC9S08QB8 ADC current consumption temperature sensor</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QB8-ADC-current-consumption-temperature-sensor/m-p/235828#M19486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;ADDRESS&gt;I have got some questions about the ADC module and it´s current consumption of the MC9S08QB8. Table8 on page14 of the datasheet (rev3, 3/2009) says, that the "Run suppy current - FEI mode, all modules on" at 1MHz and 3V is typically about 0.8mA. I will not be able to run the MCU in any LowPower-Modes, because there a continuous calculations to do.&lt;/ADDRESS&gt;&lt;P&gt;My questions now:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) does "all modules on" include the ADC with it´s current consumption?&lt;/P&gt;&lt;P&gt;2) if not, do I have to add the ADC specific supply currents (page22) to the 0.8mA?&lt;/P&gt;&lt;P&gt;3) does every of the 8 ADC channel take current or are those characteristics for the whole ADC module?&lt;/P&gt;&lt;P&gt;4) does the TemperatureSensor take additional current or does it behave like a 'normal' channel?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance. Regards.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Benjamin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2013 14:36:57 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2013-01-24T14:36:57Z</dc:date>
    <item>
      <title>MC9S08QB8 ADC current consumption temperature sensor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QB8-ADC-current-consumption-temperature-sensor/m-p/235828#M19486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;ADDRESS&gt;I have got some questions about the ADC module and it´s current consumption of the MC9S08QB8. Table8 on page14 of the datasheet (rev3, 3/2009) says, that the "Run suppy current - FEI mode, all modules on" at 1MHz and 3V is typically about 0.8mA. I will not be able to run the MCU in any LowPower-Modes, because there a continuous calculations to do.&lt;/ADDRESS&gt;&lt;P&gt;My questions now:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) does "all modules on" include the ADC with it´s current consumption?&lt;/P&gt;&lt;P&gt;2) if not, do I have to add the ADC specific supply currents (page22) to the 0.8mA?&lt;/P&gt;&lt;P&gt;3) does every of the 8 ADC channel take current or are those characteristics for the whole ADC module?&lt;/P&gt;&lt;P&gt;4) does the TemperatureSensor take additional current or does it behave like a 'normal' channel?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance. Regards.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Benjamin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 14:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QB8-ADC-current-consumption-temperature-sensor/m-p/235828#M19486</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-01-24T14:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QB8 ADC current consumption temperature sensor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QB8-ADC-current-consumption-temperature-sensor/m-p/235829#M19487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi Ben,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for my experience here is:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;All modules obviously includes ADC. In case 3V/1MHz Is=0.8mA, presumably with ADC is in its lower power state.&lt;/LI&gt;&lt;LI&gt;No if not in high speed, short sample. I think 0.8mA total supply is "typical" i.e. minimum or intermediate state regarding ADC power sink&lt;/LI&gt;&lt;LI&gt;No. only one channel is active each time, the others are high impedance state&lt;/LI&gt;&lt;LI&gt;No. Temperature sensor bias is only few uA and this is included in the ADC supply.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Salvatore&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2013 23:38:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QB8-ADC-current-consumption-temperature-sensor/m-p/235829#M19487</guid>
      <dc:creator>Encoder1</dc:creator>
      <dc:date>2013-01-24T23:38:20Z</dc:date>
    </item>
  </channel>
</rss>