<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Programming/reading/erasing MC68HC908MR32 FLASH in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129414#M1948</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi everybody.&lt;/DIV&gt;&lt;DIV&gt;The target in my firmware application is read/write operations on 32KB MR32 µC.&lt;/DIV&gt;&lt;DIV&gt;I follow AN2183 ( &lt;STRONG&gt;&lt;SPAN style=": ; font-size: 2; font-family: Arial;"&gt;Using FLASH as EEPROM on the MC68HC908GP32&lt;/SPAN&gt;&lt;/STRONG&gt; )&amp;nbsp;and AN2183SW to implement&amp;nbsp;the features, in fact&amp;nbsp; either the GP32 µC and MR32 one have no embedded ROM routines to use for writing and reading flash memory.&lt;/DIV&gt;&lt;DIV&gt;First of all, I would like to know if this application note is the one I can consider for my operations.&lt;/DIV&gt;&lt;DIV&gt;Besides, I tried to make a Code Warrior Project for GP32 to use directly AN2183SW &lt;SPAN&gt;algorithm, but I get some errors when I build the project because the CASM08 used by Code Warrior doesn't recognize for example "{ }", logical symbols like " | " and so on. Could anybody tell me why?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Mar 2006 16:03:50 GMT</pubDate>
    <dc:creator>fra</dc:creator>
    <dc:date>2006-03-21T16:03:50Z</dc:date>
    <item>
      <title>Programming/reading/erasing MC68HC908MR32 FLASH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129414#M1948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi everybody.&lt;/DIV&gt;&lt;DIV&gt;The target in my firmware application is read/write operations on 32KB MR32 µC.&lt;/DIV&gt;&lt;DIV&gt;I follow AN2183 ( &lt;STRONG&gt;&lt;SPAN style=": ; font-size: 2; font-family: Arial;"&gt;Using FLASH as EEPROM on the MC68HC908GP32&lt;/SPAN&gt;&lt;/STRONG&gt; )&amp;nbsp;and AN2183SW to implement&amp;nbsp;the features, in fact&amp;nbsp; either the GP32 µC and MR32 one have no embedded ROM routines to use for writing and reading flash memory.&lt;/DIV&gt;&lt;DIV&gt;First of all, I would like to know if this application note is the one I can consider for my operations.&lt;/DIV&gt;&lt;DIV&gt;Besides, I tried to make a Code Warrior Project for GP32 to use directly AN2183SW &lt;SPAN&gt;algorithm, but I get some errors when I build the project because the CASM08 used by Code Warrior doesn't recognize for example "{ }", logical symbols like " | " and so on. Could anybody tell me why?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Mar 2006 16:03:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129414#M1948</guid>
      <dc:creator>fra</dc:creator>
      <dc:date>2006-03-21T16:03:50Z</dc:date>
    </item>
    <item>
      <title>Re: Programming/reading/erasing MC68HC908MR32 FLASH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129415#M1949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi, I wonder if HC08 Bootloader appnote (AN2295) may help you with in-circuit Flash programming. MR32 too is supported so looking into bootloader sources you can find the actual code for Flash programming.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Pavel, ok2ucx (AN2295 developer)&lt;/P&gt;&lt;P&gt;Freescale Roznov, CZ&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2006 15:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129415#M1949</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2006-03-23T15:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: Programming/reading/erasing MC68HC908MR32 FLASH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129416#M1950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi FRA,&lt;/P&gt;&lt;P&gt;I doubt wether i ve clearly understood ur question. Wats ur ultimate aim? Is it to erase and program MC68HC908MR32's flash using ur custom built hardware (MR32==&amp;gt;RS-232==&amp;gt;PC==&amp;gt;Code warrior)&amp;nbsp;&amp;nbsp;and Code warrior?&lt;/P&gt;&lt;P&gt;Well I have jus gone thro this and now I&amp;nbsp;hav successfully erased and programmed MR32. I am also able to debeug my code, ADC, IO ports...&lt;/P&gt;&lt;P&gt;&amp;nbsp;For this all u need is to download the datasheet MC68HC908MR32_Rev_6.1.pdf.&lt;/P&gt;&lt;P&gt;Then&amp;nbsp;pg 257 gives a Monitor mode entry&amp;nbsp;circuit.&amp;nbsp; Some minor changes in the circuit will help u to do wat u intend...&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;ViVek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2006 13:46:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129416#M1950</guid>
      <dc:creator>vivek</dc:creator>
      <dc:date>2006-03-24T13:46:48Z</dc:date>
    </item>
    <item>
      <title>Re: Programming/reading/erasing MC68HC908MR32 FLASH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129417#M1951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi ViVek, thanks for the reply. You're right, &lt;SPAN&gt;perhaps I explained the problem not clearly. My goal is to write, read and erase MR32's FLASH run-time: I need to store some dates while my application is running, so that the control board can remember it after a supply fault, for example. In this way I could&amp;nbsp; use FLASH memory like an EEPROM one, isn't it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I know MR32 datasheet, I think it's not &lt;SPAN&gt;enough to implement this feature. A valid help is AN2183 and I would like get other documents, if they exist.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2006 15:47:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-reading-erasing-MC68HC908MR32-FLASH/m-p/129417#M1951</guid>
      <dc:creator>fra</dc:creator>
      <dc:date>2006-03-24T15:47:53Z</dc:date>
    </item>
  </channel>
</rss>