<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: M9KA2 marking code on a SOIC 8</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9KA2-marking-code-on-a-SOIC-8/m-p/233004#M19425</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It could be a new marking but the SOIC KA2's I have are marked with M9RS8KA2.&amp;nbsp; Do you see the little Freescale logo (looks like steps)?&amp;nbsp; There also should be 2 more lines of text.&amp;nbsp; The first is a letter code and the bottom is a date code. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2013 13:32:31 GMT</pubDate>
    <dc:creator>lydia_ziegler</dc:creator>
    <dc:date>2013-02-21T13:32:31Z</dc:date>
    <item>
      <title>M9KA2 marking code on a SOIC 8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9KA2-marking-code-on-a-SOIC-8/m-p/233003#M19424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a circuit with a SOIC 8 IC marked with the code M9KA2. I think it is a Freescale microcontroller, but I'm not sure.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could it be MC9RS08KA2?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2013 08:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M9KA2-marking-code-on-a-SOIC-8/m-p/233003#M19424</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-01-22T08:17:20Z</dc:date>
    </item>
    <item>
      <title>Re: M9KA2 marking code on a SOIC 8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9KA2-marking-code-on-a-SOIC-8/m-p/233004#M19425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It could be a new marking but the SOIC KA2's I have are marked with M9RS8KA2.&amp;nbsp; Do you see the little Freescale logo (looks like steps)?&amp;nbsp; There also should be 2 more lines of text.&amp;nbsp; The first is a letter code and the bottom is a date code. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2013 13:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M9KA2-marking-code-on-a-SOIC-8/m-p/233004#M19425</guid>
      <dc:creator>lydia_ziegler</dc:creator>
      <dc:date>2013-02-21T13:32:31Z</dc:date>
    </item>
    <item>
      <title>Re: M9KA2 marking code on a SOIC 8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9KA2-marking-code-on-a-SOIC-8/m-p/233005#M19426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I have a board designed a couple of years ago with that part and the component is marked M9KA2, next line is RMAKDC. Part is a MC9S08KA2 in SOIC8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--Rafa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2013 16:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M9KA2-marking-code-on-a-SOIC-8/m-p/233005#M19426</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-02-21T16:21:47Z</dc:date>
    </item>
  </channel>
</rss>