<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The TOF status flag doesn't seem right in a S08TPMV3 type module of an SH8. in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/The-TOF-status-flag-doesn-t-seem-right-in-a-S08TPMV3-type-module/m-p/230686#M19395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is ported code from a working project using 908QY4. I can't seem to get the TPM TOF to be set at proper values.&lt;/P&gt;&lt;P&gt;I load the modulo $FFFE, then time an event based on not overflowing at a particular prescale value. On overflow, I set the prescale higher and retime.&lt;/P&gt;&lt;P&gt;I'd use the MTIM (Boy does that look like the QY TPM), but it's 8 bit, I need 16.&lt;/P&gt;&lt;P&gt;The TOF is being set not by any predictable manner I can see, sure isn't modulo overflow. Somebody got a clue for me? TNX &amp;lt;&amp;lt;&amp;lt;)))&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Jan 2014 22:22:08 GMT</pubDate>
    <dc:creator>CustomSarge</dc:creator>
    <dc:date>2014-01-12T22:22:08Z</dc:date>
    <item>
      <title>The TOF status flag doesn't seem right in a S08TPMV3 type module of an SH8.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/The-TOF-status-flag-doesn-t-seem-right-in-a-S08TPMV3-type-module/m-p/230686#M19395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is ported code from a working project using 908QY4. I can't seem to get the TPM TOF to be set at proper values.&lt;/P&gt;&lt;P&gt;I load the modulo $FFFE, then time an event based on not overflowing at a particular prescale value. On overflow, I set the prescale higher and retime.&lt;/P&gt;&lt;P&gt;I'd use the MTIM (Boy does that look like the QY TPM), but it's 8 bit, I need 16.&lt;/P&gt;&lt;P&gt;The TOF is being set not by any predictable manner I can see, sure isn't modulo overflow. Somebody got a clue for me? TNX &amp;lt;&amp;lt;&amp;lt;)))&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jan 2014 22:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/The-TOF-status-flag-doesn-t-seem-right-in-a-S08TPMV3-type-module/m-p/230686#M19395</guid>
      <dc:creator>CustomSarge</dc:creator>
      <dc:date>2014-01-12T22:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: The TOF status flag doesn't seem right in a S08TPMV3 type module of an SH8.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/The-TOF-status-flag-doesn-t-seem-right-in-a-S08TPMV3-type-module/m-p/230687#M19396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sargent,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your code is expected. one point you may take care:&lt;/P&gt;&lt;P&gt;1. TPMv3 get a coherency mechanism that means some registers like modulo, channel value...can't be updated immediately if CLKSB:CLKSA not = 0:0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Weiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 09:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/The-TOF-status-flag-doesn-t-seem-right-in-a-S08TPMV3-type-module/m-p/230687#M19396</guid>
      <dc:creator>weapon</dc:creator>
      <dc:date>2014-01-22T09:15:05Z</dc:date>
    </item>
  </channel>
</rss>